View Full Version : HR-OS1 Development and Discussion
- [News/Announcement] HR-OS1 Documentation
- Welcome HR-OS1 Beta Testers! Introduce yourself
- [News/Announcement] Shipment Status
- Building one from scratch?
- Walk Mode balance issue
- Dynamixel error - no torque + red light blinking
- [Question(s)] Motor Connection Issues
- Walk Tuning - Discussion and Notes
- Abotix Pros - Troubleshoot
- [Question(s)] Can you use R+ Motion with HR-OS1?
- Raspberry Pi 2 image recovery + HR-OS1 Framework
- [Just For Fun] Poses - Hello World
- Arbotix Pro Pin Out diagram and JTAG Programming Guide
- [Discussion] Kit Comments/Suggestions
- Camer is built but were to plug it in.
- [Discussion] It sits, it stands, what next?
- Google Hangouts HR-OS1 Beta Development Open House
- [Question(s)] ps3_demo and Edison libusb-0.1.so.4
- HR-OS1 3D Models & 3D Printed Armor
- [News/Announcement] Fixed Camera Wiring Diagram
- [Bioloid] HR-OS1 Battery check Low Voltage warning FIX
- Streaming camera view?
- Using PS3 controller code...
- Mixing Dynamixel Servo (4 pin & 3pin) on Arbotix Pro
- Offset question?
- 50 Lucky people with beta units... now what?
- Speakers?
- Build and Documentation feedback, how should we give it?
- learn.trossenrobotics.com links to HR-OS1 docs are broken.
- node_server example
- HROS1 Simulator, is Darwin OP similar enough?
- hobby pwm micro servo on Arbotix pro
- Remove Compiler Warnings from HR-OS1 framework...
- 3D Printed Endoskeleton
- Servos not working
- Beta Tester Roll Call
- Broken part -- needing replacement
- [News/Announcement] The Next Round of HR-OS1 Beta Kits is available!
- [Project] Beginnings of ROS on the HROS-1/Hello from University
- Arbotix-Pro doesn't recognize servos
- [Project] WinRME ( Robot Motion Editor for Windows )
- Semi-Scratch Built HROS1 Inspiratron (baymax vs .001)
- 3D printable models for the HR-OS1
- HROS-1 with ODROID XU4
- Trying to debug HROS1 with RPI talking to Arbotix Pro
- Camera / Vision Processing (within the HR-OS1 Framework)
- Driving HROS1 with Kinect
- Coding standards?
- Missing bits ,,,
- My HR OS-1 falls a lot, can't pair PS3 to Intel Edison
- Problems with Arbotix Pro connecting to servos
- Edison PS2 Controller Bluetooth Issues
- HROS-1 Leaning Forward
- [Discussion] When setting the ID for the servos, you need to scan twice to find it
- Head Tilt Range
- Bracket F4 and 3D Printed Armour
- Just wondering which processor people are using?
- Conflict between rme and ps3_demo in using the CM 730
- Why we need to have the customized webcamera cable, not using the standard USB cable?
- Extending the Motion Repertoire of OS1
- motion_4096, motion_dest, motion_src, what are these files for?
- node_server update?
- Walk Tuner Tutorial?
- [Project] DIY FSR Feet for the HR-OS1
- Indiegogo - Alpha 2
- Add offset to servo positions?
- [Interesting] Raspberry Pi custom services
- HR-OS1 + Pi Zero (HR-OS-Zero?)
- Experiment - 3d printing hands with Neopixel...
- [DEMO] walking on stairs!
- Problems with 'git checkout master'
- [Question(s)] Integrate walking and RME as a single ROS module?
- HR-OS1 angular velocity and linear acceleration estimate
- [Question(s)] HR-OS1 Has anyone added additional servos ?
- [Question(s)] dxl_monitor Access or Range Error
- IMU support - Next gen Arbotiix Pro/ or Playing with my Teensy version of Arbotix-pro...
- [Interesting] RPI3 with the HROS1-Framework.
- How useful it is to use ROS?
- Any Method to Check If A Servo Needs to Be Replaced?
- HR-OS1 shaking when standing
- Changes to Walking
- HR-OS1 just getting started
- The name of the material for HROS parts?
- Adding RME actions to Vision Processing
- [Question(s)] Arbotix Pro erratic after apt-get update & upgrade on my RPI3
- [Bioloid] Issues connecting Odroid XU4 to Arbotix Pro
- Actuators blinking RED upon boot
- Planning to build HR-OS1 robot using AX-12A & AX-18A (looking for frames)
Powered by vBulletin® Version 4.2.3 Copyright © 2021 vBulletin Solutions, Inc. All rights reserved.