PDA

View Full Version : Question regarding USB output/microcontroller


peddamat
06-13-2007, 06:14 PM
Hello All,

I was wondering what the USB outputs are used for on the InterfaceKit 8/8/8? Are the differential pins connected to the microcontroller? Which microcontroller is used on the board (to see if there are any existing SDKs).


Thanks,

Sumanth P.

Alex
06-15-2007, 04:50 PM
The USB outputs are nothing more than a USB hub. In order to use it, you need the power supply:

http://www.trossenrobotics.com/store/p/3442-Power-Supply-USA.aspx

That one is only for US style outlets. We have many others, just run a search for "power supply".

The microcontroller used on the board is not accessible outside of the Phidget API. You can't pre-program the board, it's a slave device.

You can use this and all other Phidget devices in all major programming environments (C, C++, .NET, Java, etc.) All of the API's are available here (http://www.phidgets.com/modules.php?op=modload&name=Downloads&file=index&req=viewdownload&cid=3)