View Full Version : Transformers... more than meets the eye
BauerMECH
07-02-2007, 11:08 AM
New Robonova-1 skin... Gerneration 1 version of Optimus Prime! (the version I grew up with) A few additional details and He'll be ready to go with us to the movies! :)
http://robosavvy.com/Builders/bauermech/Optimus-Prime-5.jpg
http://robosavvy.com/Builders/bauermech/OP6.jpg
DUDE, that has got to be the coolest skin mod I've ever seen! So appropriate:
http://www.transformersmovie.com/
I can't wait for the movie:D
Wow, that's awesome! Thanks for doing this, Matt. You're a credit to our generation.
crabfu
07-03-2007, 12:50 PM
That is WAY too cool Matt, G1!!!!!! too cool, great job! can't wait to see it in action :)
Mini Transformers Review (couple of tiny spoilers)
Man, I just saw the new Transformers movie last night! I gotta say, Michael Bay (MB) didn't do too shabby of a job. I was expecting him to totally ruin my childhood by pissing all over the Transformers (there was a funny scene where a dog pissed over an Autobots foot though, haha), but he didn't, at least not that much;) I could've slapped him for certain scenes, but overall, I really enjoyed the movie. I do have to admit though, above all, the one thing that irked me a bit was the camera angles and focus. It was like someone had a regular camcorder and didn't know where to point the damn camera.
I mean sure there were the typical things wrong with every movie that I've just became accustomed to expecting when watching a movie: holes in the plot, goofy scenes that could've had more thought put into them, then the things that MB should have been slapped for doing to transformers: the fact that there were more humans in the movie than transformers, a bit too cheesy of lines. But, I mean come on, when ya only have xx amount of time to cram xx amount of content into a movie, there are going to be flaws, right?
But, overall, I'd give it a B, maybe a B+. Definitely worth watching, imo:)
Did anyone else get a chance to check it out yet? What'd ya think?
vBulletin® v3.8.1, Copyright ©2000-2010, Jelsoft Enterprises Ltd.