PDA

View Full Version : Power Control System



SkipFire
07-23-2007, 04:50 PM
I have built a power control system that uses relays to temporarily close power and reset buttons on an ATX computer, and can interrupt the power coming into the computer. It also has an IFK that plugs into the power LED pins on the motherboard to provide feedback on the current power state of the computer. The components are all connected to an Ethernet connected XScale Windows CE computer and uses a telnet server to allow remote connections to control and monitor the system.