BillW
08-09-2007, 03:39 PM
What I'm looking for is a servo that turns much more than the ~200 degrees that mine turn but still allows exact positioning. I'm looking for more like 1000 degrees but, other than some very expensive servos for sailboats, there doesn't seem to be such a thing. I have the Phidgets 4 servo controller and have confirmed that I can move in tenths of a degree. (maybe smaller but this is good enough for me) Geared 500% it would still be more than granular enough for my uses.
I had some continuously rotating servos on back-order but they have been discontinued. I was never sure they would work for me anyway because it didn't sound like they'd give me the exact positioning I wanted.
So:
Can I gear up the servo inside the servo case so that I can tell it to sweep more than the ~200 degrees or is the sensing portion of the servo tied to the angle of the output? Are there gears to even do this?
If I can't do it inside then does anyone reading this know of somewhere I can find gears to step up the rotation outside the servo? (I've been hoping to find a gear project kit that supplies gears and handy things to have properly oriented shafts, etc. I did get a meccano set but it unfortunately only has pulleys.)
Thanks. :)
I had some continuously rotating servos on back-order but they have been discontinued. I was never sure they would work for me anyway because it didn't sound like they'd give me the exact positioning I wanted.
So:
Can I gear up the servo inside the servo case so that I can tell it to sweep more than the ~200 degrees or is the sensing portion of the servo tied to the angle of the output? Are there gears to even do this?
If I can't do it inside then does anyone reading this know of somewhere I can find gears to step up the rotation outside the servo? (I've been hoping to find a gear project kit that supplies gears and handy things to have properly oriented shafts, etc. I did get a meccano set but it unfortunately only has pulleys.)
Thanks. :)