FeralBot
09-04-2007, 07:34 PM
Hello,
I own a Pololu micro serial controller. Can the Pololu serial controller be detected and used with the Phidget web server? I have it plugged in, but it is not detected. This seems of course that I only have the RS-232 input cable connected. (Output but no input)
Should I be using the Logic Level input/output instead, or am I totally off course? Do I need to buy a Phidget compatible servo controller?
Thanks for any help.
I own a Pololu micro serial controller. Can the Pololu serial controller be detected and used with the Phidget web server? I have it plugged in, but it is not detected. This seems of course that I only have the RS-232 input cable connected. (Output but no input)
Should I be using the Logic Level input/output instead, or am I totally off course? Do I need to buy a Phidget compatible servo controller?
Thanks for any help.