View Full Version : Robophilo
Droid Works
09-13-2007, 10:31 PM
Coming soon ! http://robophilo.com .
Nice find.
Man, humanoids are coming out so fast that we can't keep up anymore! This is the first I've seen of this and we sell them all, LOL.
It's certainly sounds intriguing, but there's no contact info anywhere to be found and half the links on the site go to missing.html. We would be interested in talking to them to see if it would be worth carrying. If anyone finds a contact let us know.
Droid Works
09-14-2007, 02:09 PM
I think its a great entry level humanoid. I will try to get the manufacturer info for for you.
Droid Works
09-14-2007, 02:23 PM
Its made by The World Models Manufacturing co. I will send you the phone # via PM. The site will be updated within a month. And they should be rdy for US sale before X-mas. They are having some over seas regulatory issues but I will hopefully be ironed out soon.
Droid Works
09-14-2007, 03:12 PM
http://i84.photobucket.com/albums/k15/walice_drel/more4.jpg
cdraptor
09-22-2007, 11:48 PM
Droid - do you know any specs on the servos, it sounds like it will be an impressive robot for the price, but I wonder how they're hitting the pricing. Since servos typically make up the bulk of the cost - cheaper servos would keep the price down I mean you look at a decent servo for a typical humanoid and $30 - 40 is fairly low end in power for full humanoid - which your talking in the 600 - 800 just for servos. Sounds almost to good to be true.
It's being made in China. That's one cost reducer right there.
Droid Works
09-23-2007, 01:08 AM
Give me a call when you get a chance and I will give you an update.
Droid Works
09-23-2007, 01:10 PM
There are some new pics fo the Robophilo on the Robophilo web site:)
Pretty decent specs for a $500 robot:
Height: 13" ( 330.2mm )
Weight: 1.2kg ( 1200g ) with battery
PCB Unit
- Dimensions: 2.99" x 2.24" x 0.06" ( 76 x 57 x 1.6mm )
- Weight: 1.91oz ( 54g )
- Operating Voltage: 6V DC
- CPU: Atmega32 - 16PU
SV 4032 Servos
- Dimensions: 1.59"L x 0.78"W x 1.42"H ( 40.4 x 19.8 x 36mm )
- Weight: 1.3oz ( 37.2g )
- Torque: 4.1kg-cm
- Speed: 0.19 sec/60°
- Operating Voltage: 6V DC
SV 4104 Servos
- Dimensions: 1.57" x 0.79" x 1.5" ( 40 x 20 x 38.1mm )
- Weight: 1.4oz ( 41g )
- Torque: 6.5kg-cm
- Speed: 0.16 sec/60°
- Operating Voltage: 6V DC
SV 2030 Servos
- Dimensions: 0.89" x 0.45" x 0.81" ( 22.8 x 11.5 x 20.8mm )
- Weight: 0.28oz ( 8g )
- Torque: 1.3kg-cm
- Speed: 0.12 sec/60°
- Operating Voltage: 6V DC
7.2V 1000mA Charger
- Input: AC 100 - 240V, 50/60Hz 500mA
- Output: 7.2V 1000mA
- Dimensions: 1.69" x 2.91" x 1.33" ( 43 x 74 x 34mm )
- Weight: 100g
- Charging Time: Approximately 1.5 hrs
6V Ni-MH 5 x 2/3AA 700mAh Battery
- Dimensions: 1.14" x 1.57" x 1.14" ( 29 x 40 x 29mm )
- Weight: 75g
- Voltage: 6V
- Capacity: 700mAh
Where are these new pics you're referring to though? I couldn't find them anywhere. They have a pretty slick site going on (yes, this is the first time I checked it out).
Droid Works
09-23-2007, 11:09 PM
Clicek on events then gallery.
http://i84.photobucket.com/albums/k15/walice_drel/robophilo.jpg
srobot
09-28-2007, 06:33 PM
If anyone finds a contact let us know.
This is on page 89 in Fall Robot Magazine.
Phone:
(925)-371- #take this out# 0922
--Scotty
Thanks Scotty:) Surprisingly, I must've completely missed that ad every time I opened up that issue, haha!
jahnnex
10-21-2007, 10:29 AM
Does any one know when the RoboPhilo will be available for sale? I saw it at the IHobby Show this weekend and it was quite impressive.
not too sure on when it will be available. Matt was talking to the guys that created the RoboPhilo at iHobby, so he might be able to shed some light on this. I do know that once it is, we'll be carrying it:) It is a pretty cool robot, huh? Keep an eye out on our blog because we'll have a writeup on it once we finish editing the video.
What did you like best about it?
tom_chang79
02-07-2008, 02:28 PM
Are the brackets for the Robophilo made of plastic or aluminum?
Tyberius
02-07-2008, 02:36 PM
Plastic for sure. At that cost I don't see how they could afford to use aluminum.
yep, they're made of Plastic. It is a budget bot, but definitely really cool.
jahnnex
02-08-2008, 08:52 AM
It is definitely a good bot if you are new to humanoids. I am thinking about buying another one just because of the cost.
vBulletin® v3.8.1, Copyright ©2000-2010, Jelsoft Enterprises Ltd.