PDA

View Full Version : What power source?



jdolecki
10-12-2007, 08:29 PM
I was wondering what would be the best way to power a PC based robot.

I was thinking od hacking a UPS system for the guts, or if some one could suggest something better.

thanks
john

Migs
10-13-2007, 08:36 AM
Hi Abacus:
Buy a battery pack from Trossen or Lynxmotion. Size it to match your motor speed controller (like a Sabertooth, or for the Servos on your servo controller). It is best to submit to the people here your final motor count (amps) or qty of servos and other components so you see if you have enough juice. (Also so your controller is matched properly). Since you might not know what batteries are in a UPS, you can goof it if say you have more cells than the controller can handle. Also: Some motor controllers are battery TYPE specific, and they have dip switch positions to reflect your choice. If you don't know what your batteries are then this could lead to a problem. I would also think that the UPS batteries, meant to deliver 115 Volts eventually through conversion may be too bulky for your robot. Trossen has flat battery packs that are really nice to use and not expensive at all. Also, consider getting a good battery charger like the Duratrax Intellipeak Charger, because these can be programmed for the exact battery you are charging:
http://www.duratrax.com/caraccys/dtxp4170.html

All the best, -Migs

jdolecki
10-13-2007, 03:22 PM
Right now i just want to power my motherboard. I was going to use a laptop for my brain but I have this spare motherboard that will be dedicated to just the robot. So if I could get about 2-3 hours of on time that would be great. My drives will all have there own power source.

Is there a premade unit that will interface a battery to a motherboard?

Matt
10-13-2007, 05:24 PM
Hey John,

I believe what you are looking for is a DC to DC converter. These are made for smoothing out battery power for use with computer boards. Logic Supply is the place to go :)
http://www.logicsupply.com/categories/power_supplies

jdolecki
10-17-2007, 04:41 PM
Does anybody know how many watts a full size motherboard draw? What about a Hard Drive?

Thanks
John

Migs
10-18-2007, 06:44 AM
John:

These guys would probably be able to tell you:
http://www.logicsupply.com/

Migs

jdolecki
10-18-2007, 06:14 PM
I talked to Logic supply tech support.
1. a full size motherboard running a core2 processor is 110w at 100%
2. a full size motherboard running a p4 is about 170w at 100%

Here is what if found. ALthough it not a "Smart" power supply is is 200w.

http://www.mini-box.com/s.nl/sc.8/category.13/.f

jdolecki
10-18-2007, 06:15 PM
And its only $48 dollars.