cdraptor
10-13-2007, 05:58 PM
The Speecys SPC-101C has an SDK called Open Roads - I have been working on translating the documentation, understanding the calls and building my own C# wrapper to simplify using the SPC-101C. The Open Roads SDK is a very powerful and relatively simple approach - you communicate to the SPC-101C via TCP/IP socket datastreams - each command has a specific data packet format. So far from example code and question/answers with Koji at Speecys I've been able to setup in my app calls to the Motion Files and now I have a direct servo control function which you can see in this video I am using to control the neck servo by providing the angle - currently I am not setting the speed, so it's default - my next step is to provide the speed parameter. I am going to be setting up control for the midsection body servo for looking down and up.
I've added image snapshot capture to the application as well which I am planning to use with some facial recognition and object recognition libraries (more info on that to come soon). What I should be able to do now with servo control and using the object/facial libraries is to provide active object tracking for the SPC-101C. So enjoy the vid, more to come, maybe before the weekend is out
vdwlNpXA1PU
I've added image snapshot capture to the application as well which I am planning to use with some facial recognition and object recognition libraries (more info on that to come soon). What I should be able to do now with servo control and using the object/facial libraries is to provide active object tracking for the SPC-101C. So enjoy the vid, more to come, maybe before the weekend is out
vdwlNpXA1PU