PDA

View Full Version : H bridge Design


jdolecki
11-12-2007, 07:41 PM
Being the cheap person i am and needing 10 motor drivers does anybody have a h-bridge design they want to share? I have a lynxmotion ssc driveri want to use.

12vdc 3a max.

thanks

Alex
11-15-2007, 11:03 AM
Sorry, I'm not all that savvy in EE stuff, but I looked around and found a couple of sites that might at least give you a good starting point on some areas:

http://www.mcmanis.com/chuck/Robotics/tutorial/h-bridge/bjt-circuit.html

http://www.robotroom.com/HBridge.html
http://www.robotroom.com/BipolarHBridge.html


The RobotRoom has a ton of good content on there. It's just not that easy to find it all.

Hope some of that info helps:)

robot maker
07-05-2008, 09:16 PM
lm298 is a very easy circuit and dual 3 amp circuits,looking for a cheap h bridge circuit with all parts solarbotics has one in kits for $19.00 part #, kit#13

lnxfergy
07-05-2008, 09:25 PM
12VDC, 3A max, but what is the typical current? The TI SN754410 is about $1.50 a chip, and controls two motors (so 5 chips for your 10 motors). BUT.... it is rated 1amp continuous, 2amp peak (3-36VDC). If I remember correctly, that is without a heatsink. It may be possible with a heat sink to pull 3A, but I'm not sure.... testing would be required. If the SN754410 won't do 3amps without blowing, the L298 is probably the next lowest cost single-chip motor driver (it is 3A rated, but runs about $3 per motor channel).

As far as using the SSC32 with these motor drivers - that is likely going to increase the cost. You are going to need a circuit to change servo pulses to motor voltage. I know there are few out there on the web, but as far as I remember, each circuit needs about 2-3 different TTL chips, by the time you get done building a 10 channel version you can figure to have 20 TTL chips, and about the same number of resistors and caps. A nightmare to debug....

What exactly are you building that requires 10 channels?

-Fergs

Edit: Wow, just noticed that the original thread was from Nov 07. Guessing this info won't be useful to the original poster (unless his projects progress as slow as mine...)