PDA

View Full Version : [Contest Entry] Sandman Robot!



Greathouselabs
11-17-2007, 01:58 PM
The Sandman is an 800lb walking robot with 16 separate remote controlled movements. He has a Gasoline and propane flamethrower in front and a gasoline machine gun mounted in the rear. When his mouth is extended his total length is around 11'

He has Harley Davidson exhaust pipes mounted on his sides capable of shooting 15 ' flames. The front flame thrower capable of shooting flames 20'. He is operated using two Futaba Helicopter radios.

96

97

He is used for various entertainment events.


http://www.youtube.com/watch?v=_mmDRiK-MDE

Unfortunately, this does not show him walking,.

Sandman uses a small victor speed controller for driving the two wheelchair motors for forward and backward movement. All the control system were handmade using old magnetic tape drive computer parts, servos, relays,micro switches and motors. The mouth is extended and retracted using a boat hand winch. I modified the winch by adding an electric motor and several tilt switches. He carries a SCUBA and propane tank inside for running his pneumatics and flamethrowers. Two diesel electric batteries are mounted under his pivoting front end for 24 volt electrical power. Gasoline can be injected into the flamethrowers with a flip of a switch.

Movements

Walking Forward Backward Left Right
Mouth Extend,Retract, Open ,Close,Left,Right
Mandibles Open,Close
Ribs Up, Down
Wings In,Out
Heads Left, Right

Lance

More information and videos on him listed on.
www.racegreathouselabs.com (http://www.racegreathouselabs.com)

Alex
11-26-2007, 02:54 PM
Didn't realize that I haven't replied yet, my bad:(

Pretty cool amazing robot Lance, great work! I have you entered in our contest.

Dave
11-28-2007, 04:27 PM
All I can say is this: we don't get nearly enough 800 lb fire-spewing robots in these forums. Bravo!