bryanhou
12-03-2007, 06:35 PM
Hi All,
Can the RW-210 read multiple tags simultaneously?
I'm using the test application from APSX. Both the getUID and fastGetUID methods return false if more than one tag is detected.
Is this a limitation of this reader? Or am I missing some other method (or some other DLL) that can return multiple UIDs if there are multiple tags detected?
Cheers.
Can the RW-210 read multiple tags simultaneously?
I'm using the test application from APSX. Both the getUID and fastGetUID methods return false if more than one tag is detected.
Is this a limitation of this reader? Or am I missing some other method (or some other DLL) that can return multiple UIDs if there are multiple tags detected?
Cheers.