View Full Version : Touch sensitivity
electrocute
12-11-2007, 03:09 PM
What kind of sensors to be used for implementing touch sensitivity. So that the specific bot part retracts itself after sensing touch.
jdolecki
12-11-2007, 03:57 PM
http://www.trossenrobotics.com/store/c/2670-Force-Sensors-Pressure-Touch-Sensors.aspx
kdwyer
12-11-2007, 08:04 PM
A simple push-button could also work, with an attached bumper. Might be easier to read, too. And cheaper to implement.
Cheaper + easier = Better (usually)
I must be the laziest bot-builder ever!
Tymtravler
12-12-2007, 06:49 AM
Hey Electrocute
What is the application for, is it for a gripper? More input needed to solve question.
Tymtravler
vBulletin® v3.8.1, Copyright ©2000-2010, Jelsoft Enterprises Ltd.