tom_chang79
02-05-2008, 09:19 AM
Hello, was wondering if you 1HV owners can answer these questions:
1) Are the servo brackets made of plastic?
2) Are there any 1HV kits sold without the packaged servo? In case I would like to buy this kit with more powerful servos up front rather then replace the default ones without ever using them?
3) I've read that 1HV shipped with an older firmware on the robot controller board (v 1.03), are the kits on robosavvy now shipping with the latest firmware? If not, can the firmware be upgraded over the internet, i.e. download, etc...?
1) Are the servo brackets made of plastic?
2) Are there any 1HV kits sold without the packaged servo? In case I would like to buy this kit with more powerful servos up front rather then replace the default ones without ever using them?
3) I've read that 1HV shipped with an older firmware on the robot controller board (v 1.03), are the kits on robosavvy now shipping with the latest firmware? If not, can the firmware be upgraded over the internet, i.e. download, etc...?