mterm
02-08-2008, 06:50 AM
I am new to using this product and confused with how to set up the 4 servo controller with (2) hitech 815BB servos. The wiring is not the issue I am using a separate power supply for the servos. The problem is I am not sure that I have properly downloaded the software and installed everything I needed to. I down loaded phidget21.msi and installed it but I did not download any of the choices in step 2 because I was not sure what language to choose. I can get phidget21 to run, the PH in the bottom right hand corner of the screen and I can get the servoful tab and use the slider to control the servos. But is that all the control I should have. Is there something that allows me to control the speed at which the servo travels. IF anyone could point me in the right direction I would really appreciate it.
Mark:confused:
Mark:confused: