brendanburns
02-18-2008, 12:34 PM
Hello,
Fernando Orellana and I (Brendan Burns) have created a piece of robotic art entitled "Sleep Waking" (http://www.fernandoorellana.com) its on display at the exit art gallery (http://exitart.org) in Manhattan until April 19th.
Using recorded brainwave activity and eye movements during REM sleep to determine robot behaviors and head positions, "Sleep Waking" acts as a way to "play-back" dreams. Through this piece we hope to investigate one of the possible human-robot relationships.
Video:
1RkM1Bt2b3k
Technical Details:
The robot is a modified KHR-2HV with 2 Gyros and an accelerometer (to detect falls) It is hard wired into a power source so that it can run for a extended period of time (it will be on display for 2 months!)
An overhead camera (not pictured in the video) is used to provide robot position/orientation data so that it can navigate around the pedestal without falling off.
The recorded eye muscle movements are used to drive head motion, so the head movement is a literal representation of Fernando's recorded eye movement. We also used machine learning to find patterns in the EEG eletrode data. These patterns were mapped to specific behaviors (shown in the video) which are remembered from our dreams.
Thanks!
--brendan ^ fernando
Fernando Orellana and I (Brendan Burns) have created a piece of robotic art entitled "Sleep Waking" (http://www.fernandoorellana.com) its on display at the exit art gallery (http://exitart.org) in Manhattan until April 19th.
Using recorded brainwave activity and eye movements during REM sleep to determine robot behaviors and head positions, "Sleep Waking" acts as a way to "play-back" dreams. Through this piece we hope to investigate one of the possible human-robot relationships.
Video:
1RkM1Bt2b3k
Technical Details:
The robot is a modified KHR-2HV with 2 Gyros and an accelerometer (to detect falls) It is hard wired into a power source so that it can run for a extended period of time (it will be on display for 2 months!)
An overhead camera (not pictured in the video) is used to provide robot position/orientation data so that it can navigate around the pedestal without falling off.
The recorded eye muscle movements are used to drive head motion, so the head movement is a literal representation of Fernando's recorded eye movement. We also used machine learning to find patterns in the EEG eletrode data. These patterns were mapped to specific behaviors (shown in the video) which are remembered from our dreams.
Thanks!
--brendan ^ fernando