PDA

View Full Version : [Contest Entry] The Bratinator Project



SN96
02-24-2008, 08:43 AM
Here is my project submission:

I have always wanted to build my own biped robot ever since I saw the Honda robot. My biped uses 3deg. of freedom per leg and is equipped with fully functioning arms and grippers. What's unique about this project; the billet aluminum head that I designed and had custom machined. Like the arms and gripper, the head was designed to be fully functional as well. For example, the eye sockets are 16.3mm I.D. so I can mount Parallax's PING sensors in the head chassis. I have done this already by desoldering the sensors from the board using lengths of 26 gauge wires to resolder the sensors back to the board, which allows me to mount the sensor board in any location I choose. It worked fine, however, there was interference with the bridge of the nose. To fix this problem, I need to machine custom tubes to evenly shroud the sensors.

PING TESTING:

http://img141.imageshack.us/img141/6546/headtorsofronttm2.th.jpg (http://img141.imageshack.us/my.php?image=headtorsofronttm2.jpg)

The aluminum head also has the following features:

- 10mm holes on each side to mount two electret microphones for sensing sound in its
environment

http://img133.imageshack.us/img133/3184/micunder6gs.th.jpg (http://img133.imageshack.us/my.php?image=micunder6gs.jpg)

Software testing of the ears:

http://img231.imageshack.us/img231/3413/rtear1lf.th.gif (http://img231.imageshack.us/my.php?image=rtear1lf.gif)

Lexan Servo Bracket, custom designed and laser cut. Thanks Lynxmotion.

http://img164.imageshack.us/img164/9076/headbracket7kk.th.jpg (http://img164.imageshack.us/my.php?image=headbracket7kk.jpg)

http://img54.imageshack.us/img54/2091/fillerside7zl.th.jpg (http://img54.imageshack.us/my.php?image=fillerside7zl.jpg)

Video showing sound sensing and SpeakJet working together:


http://www.youtube.com/watch?v=AfJbg2Yv9DM

- 36mm mylar speaker pocket designed to mount a speaker in the underside of the head

http://img302.imageshack.us/img302/1102/speakermount8ss.th.gif (http://img302.imageshack.us/my.php?image=speakermount8ss.gif)
http://img255.imageshack.us/img255/3872/speakercableqs3.th.jpg (http://img255.imageshack.us/my.php?image=speakercableqs3.jpg)
http://img227.imageshack.us/img227/3579/mountedspeakeryr3.th.jpg (http://img227.imageshack.us/my.php?image=mountedspeakeryr3.jpg)


The custom Robotic sensor board that controls sound sensors, PING, SpeakJet, and memsic tilt sensor. Unfortunately, this board was toasted due to my carelessness. I reversed polarity on the power leads and a new board needs to be built.

http://img88.imageshack.us/img88/6798/rscurevaczx3.th.jpg (http://img88.imageshack.us/my.php?image=rscurevaczx3.jpg)

http://img414.imageshack.us/img414/3636/rcsuhighresfp9.th.jpg (http://img414.imageshack.us/my.php?image=rcsuhighresfp9.jpg)

http://img172.imageshack.us/img172/5636/bothead4yk3.th.jpg (http://img172.imageshack.us/my.php?image=bothead4yk3.jpg)

Now for the videos:


http://www.youtube.com/watch?v=m1KkLdiCSRg


http://www.youtube.com/watch?v=cl0IWHWA4u8









(http://www.youtube.com/watch?v=m1KkLdiCSRg)

Zenta
02-24-2008, 12:33 PM
Hi!

Nice work with your scull! I loved the part when he turned on his red eyes :D in your last movie.
Cool!

Alex
02-25-2008, 10:50 AM
Great job on all this SN96! Now for the questions:D

What exactly are you using the PING sensors for? They look really neat in the eye sockets, but I'm curious on their role in the system.

Did you build this custom board? If so, could you talk about your experiences with developing the board?

Care to elaborate on the software a bit?

DresnerRobotics
02-25-2008, 11:57 AM
Woohoo! Love this guy! Great job on the video!

I really need to pick up a BRAT... would love to build it as a reverse leg bot and build a mini-mech out of it. Too bad I have my eyes set on a Bioloid kit next~

SN96
02-25-2008, 05:13 PM
Great job on all this SN96! Now for the questions:D

What exactly are you using the PING sensors for? They look really neat in the eye sockets, but I'm curious on their role in the system.

Did you build this custom board? If so, could you talk about your experiences with developing the board?

Care to elaborate on the software a bit?

The ping sensors were for distance sensing. unfortunately, the sensors installed in the head did not work properly due to interference with the nose bridge. In order for the PING sensor to work properly, I found out that a tube needs to shroud the sensor evenly so the sonar is more focused. It worked well by using black construction paper curled in to 3/4" tubes and slipped over the sensors. I was not happy with this configuration so I removed them and used red LEDs for now.

The Robotic Sensor Control Unit (I called it RSCU for short) was originally designed to cut down on the mess sensors and wires can create. With bipeds there is very little real-estate for sensors unlike rovers. I decided that I wanted to custom build a board that will allow me to have all the sensors I wanted for my biped, in one neat package. Since I wanted my head to see, hear, and speak evil, a board was required to bring it all together.

The board has 3 main features for making the bot head come to life.

- SpeakJet circuit for producing speech. The SpeakJet has optional event pins that could be used with sensors. One example is the memsic sensor, where if the bot tilts to much to one side or another, a pin could be made to go "HIGH" thus calling an event that produces the phrase "Woooah!"

- Sound sensor. I had help from other members in the community to develop a simple circuit that would allow me to make my bot react to sound. I used Parallax's ADC0832 demo code to take the output of both mics and compare voltage levels. The mic with the greater voltage sensed the loudest sound.

- Memsic tilt sensor. Used for detecting orientation. With the tilt sensor, I can detect if the bot is on its back, front or leaning to much to one side or the other.

- Port for the ping sensor. This has no built in circuitry, it's only purpose was to allow quick and ease detachment of the bot head. With a port, I can simply unplug the ping wires if I need to remove the head without having to mess with anything else.

The PC board went through 5 prototypes after a bread board design, each one with improvements on the last. Some changes were just silkscreen errors, other changes were component routing errors and finally adding some component changes. The biggest improvement was the addition of the cap for the audio amp to provide more amplification. I used Eagle Cad to design my boards and BatchPCB.com to produce the fabs.

The Bratinator is using Lynxmotion's SSC-32 servo controller connected to Lynxmotions Mini ABBII. MCU of choice is the AtomPRO.

For the sequences I am using Lynxmotions SSC-32 Visual Sequencer which really helps design complex moves and sequences.

LinuxGuy
04-08-2008, 04:50 AM
I vote The Bratinator to be the biped with the most attitude and personality! Everytime I see this biped walk or perform, I marvel at what Mike has accomplished. I would love to incorporate the hearing aspect so my robot could follow the loudest sound(s) in its environment. I also very much want to add a speech synthesizer.

Well done, Mike!! :veryhappy::veryhappy:

8-Dale

airman00
08-15-2008, 05:16 PM
Very nice project!

Can you please upload your code for this project or at least PM me it . I am working with a BRAT robot as well.

4mem8
08-15-2008, 11:10 PM
SN96: Well done, I love it, I am also doing a biped Mech ED209 and would love to get this to walk like a mech, so I have some work cut out for myself. Again well done.

A-Bot
08-18-2008, 04:56 PM
This is a cool project... I'd be interesting in seeing updates if there's anything new going on. :)

ROBOTMAN
04-02-2009, 02:57 PM
Sweet robot it really came together nice!

SN96
04-03-2009, 09:18 AM
<p><font color="black"><font face="Verdana">Its been a long while since I have been around. I appreciate all the positive feedback. I haven't done much with my Bratinator but I did recently charge him up and let him walk around just a few days ago. The only update I have is the development of basic moves that can be called on as subroutines in the program. </font></font></p>
<p>&nbsp;</p>
<p><font color="black"><font face="Verdana">The itch to get working with it again has returned and I would like to try getting the eyes, ears and speech working like I once had it before toasting my board. For the ears, I want to try using the Basic Stamp BS2px with the built in compare pins to see if I can get something working. I also want to get some IR LEDs for the eyes for a bare bones solution for vision.</font></font></p>
--------
vaporizer reviews (http://vaporizer.org/reviews)

SN96
07-23-2009, 12:06 PM
Project update:

I have added IR "eyes" to the skull and I also built a new sound sensor circuit that is a major improvement from the last design. The IR sensors are simple BOE Bot IR emitters and one receiver module. Instead of having two sets, I only have one set, so one emitter, and one receiver, each in its own eye socket.

I have taken video of the experiments but I'm pressed for time, so I will have to post links to them later.
________
Yamaha XT550 (http://www.cyclechaos.com/wiki/Yamaha_XT550)

EddieB
07-23-2009, 12:35 PM
hey I thought you had a new sound processor board coming for him... did that get back shelved?

SN96
07-23-2009, 01:08 PM
Yes, it?s on the shelf, but not forgotten. I have the board in Eagle, but I'm not ready to send it off just yet. I was working with other things like IR vision, sequence steps, and audio circuits.

What?s the latest on your projects(s)?
________
Yamaha FJ1100 (http://www.cyclechaos.com/wiki/Yamaha_FJ1100)

EddieB
07-23-2009, 01:36 PM
Yes, itís on the shelf, but not forgotten. I have the board in Eagle, but I'm not ready to send it off just yet. I was working with other things like IR vision, sequence steps, and audio circuits.
Whatís the latest on your projects(s)?
with rare exception the majority of the electronics / software ones stop when I head home at the end of the day. got smacked on my cycle about a month or so ago which just makes all lifes special moments all the better. :sad: bike wasn't hurt much and I can walk on the leg so it coulda been much much worse. For a few seconds there I wondered if I was gonna become a customer for some of our own products. :tongue:
I'll get around back to hobby stuff eventually... but I think you've heard that before, heh. :rolleyes:

OT, I don't remember anything really wrong with the later circuits you sent just some tweaking needed... when you want to pick it up again send them to the yahoo e-mail and I'll go through it with you again. :happy: Be neat to see yer bot strutting his stuff again.

SN96
07-23-2009, 02:12 PM
with rare exception the majority of the electronics / software ones stop when I head home at the end of the day. got smacked on my cycle about a month or so ago which just makes all lifes special moments all the better. :sad: bike wasn't hurt much and I can walk on the leg so it coulda been much much worse. For a few seconds there I wondered if I was gonna become a customer for some of our own products. :tongue:
I'll get around back to hobby stuff eventually... but I think you've heard that before, heh. :rolleyes:

OT, I don't remember anything really wrong with the later circuits you sent just some tweaking needed... when you want to pick it up again send them to the yahoo e-mail and I'll go through it with you again. :happy: Be neat to see yer bot strutting his stuff again.

I think I have it complete except for the power protection. I was not sure if I should bother with it or not since my plan was to tap into the BB2 regulated power. It would be nice though to be able to use a variety of power options which would require a regulator and power protection built in. If you have Eagle Cad, I could email the file to you.
________
Health Discussion (http://www.health-forums.org/)

EddieB
07-23-2009, 02:58 PM
If you have Eagle Cad, I could email the file to you.
lol, take a screen capture and mail that to me. :wink: