PDA

View Full Version : Picture in Post



jdolecki
03-14-2008, 08:38 PM
How do i add apicture to my post?

Alex
03-14-2008, 09:44 PM
There's a few ways. (BTW, I moved this thread to the Off Topic forum)

First of all, make sure you're in advanced mode when replying to a thread, or creating a new thread. If you see a button with "Go Advanced" below your text editor, click it and it will take you into the advanced mode.

If you have a URL for an image, then click on this button: 203

If you have images on your computer that you'd like to upload, then scroll down to see a button, "Manage Attachments". Click on this button and a new dialog will pop up prompting you to upload images from your computer, select your image, click "upload" and then close window. You can also use the URL feature here just as above.

If you used the second method, you may want to embed your image directly into your post in a certain area. To do this, again, in advanced mode and with your image already uploaded, put your cursor where you'd like the image to show up in your post, click on the paperclip looking icon (204) and select your image.

if you need anything cleared up, let me know cuz I want to be as clear as possible:)

LinuxGuy
04-07-2008, 11:25 PM
if you need anything cleared up, let me know cuz I want to be as clear as possible:)
Is there a way to reference images we have already uploaded to our gallery and have them show within a post?

8-Dale

JonHylands
04-08-2008, 06:42 AM
Yes, this is what I do all the time. Once you have the image visible in the gallery, right click on it and say "Copy Image Location". Then click on the "Insert Image" button on the post, and paste the copied URL in...

- Jon

LinuxGuy
04-08-2008, 07:26 AM
Yes, this is what I do all the time. Once you have the image visible in the gallery, right click on it and say "Copy Image Location". Then click on the "Insert Image" button on the post, and paste the copied URL in...
Ah, so easy! Thanks, Jon! :happy:

8-Dale

Alex
04-08-2008, 08:27 AM
You can also scroll down below any of your images to find the direct link, bbcode Image code, or <img> tag code. The BBCode can be copied and pasted anywhere in the TRC (posts, blogs, etc.). The <img> tag can be used anywhere where HTML code can be used on the Internet.

218

LinuxGuy
04-08-2008, 10:47 PM
You can also scroll down below any of your images to find the direct link, bbcode Image code, or <img> tag code. The BBCode can be copied and pasted anywhere in the TRC (posts, blogs, etc.). The <img> tag can be used anywhere where HTML code can be used on the Internet.
I found all of that. :happy: I added a bunch of new pictures to my blog that Andrew took of W.A.L.T.E.R. Saturday at the PARTS meeting.

8-Dale