PDA

View Full Version : [Question(s)] SRV-1 Curiosity



LinuxGuy
03-25-2008, 02:46 AM
I notice that the SRV-1 now comes with a Blackfin processor board that has 32 MB RAM adn 4 MB Flash. The Flash size seems a bit small.

Are the RAM and Flash expandable?

8-Dale

hgordon
04-15-2008, 08:36 AM
Flash is not directly expandable on-board, though we do use the SPI interface for the on-board flash, and have at least one user working on an expansion board for off-board SD memory cards that interface via SPI.

LinuxGuy
05-02-2008, 02:12 AM
Flash is not directly expandable on-board, though we do use the SPI interface for the on-board flash, and have at least one user working on an expansion board for off-board SD memory cards that interface via SPI.
Very interesting. I will have to search this info out and see what it involves. :happy:

8-Dale