PDA

View Full Version : 0-10V Output?



Wizeman
03-27-2008, 03:14 PM
Hi!

I'm wondering if there is a way to have 0-10V DC output using a Phidgets 8/8/8.

Does a Phidget motor control output 0-10V ?

Thanks,

-Vince

Alex
03-27-2008, 04:17 PM
Have you taken a look at the product manuals yet?

Phidgets Low Votage Motor Controller (http://www.phidgets.com/documentation/Phidgets/1060.pdf)

Phidgets High Current Motor Controller (http://www.phidgets.com/documentation/Phidgets/1064.pdf)

Wizeman
04-01-2008, 12:48 PM
I have, I'm just not sure if these motor controllers will do...
From what I gather, these motors output a PWM voltage which simulates a steady voltage when passed through a DC motor. The difference between a DC motor and my intended application is that my actuators take a 2-10V signal and open or close a damper (or valve) proportionally to this signal (ie.: they stop turning when the opening is proportional to the input voltage).

For example this product:
http://www.belimo.us/bellib/Damper_Actuators/TF24_SR_S.pdf

I'm afraid that sending a PWM voltage may prematurely fry this unit. Any ideas?

Wizeman
04-02-2008, 11:45 AM
I actually found a solution to my problem: several manufacturers of HVAC control actuators offer PWM actuators, so that's solved :)