PDA

View Full Version : bioloid dance routine



trey3670
04-13-2008, 09:22 PM
I have in the software a vid of the loid doing a dance routine,for the life of me I cant find this program to download to the loid,anyone else find it?

tom_chang79
04-14-2008, 01:17 AM
hey trey, I'm assuming that you got your bioloid up and running? :happy:

Well, the dance routine isn't obvious as it isn't mapped to the U, D, L, R button after you press the START button. After you select the PLAY mode and press the START button, press the START button again. The manual states that you have to clap once after you press the start button, but I didn't find that to be the case.

trey3670
04-14-2008, 06:19 PM
yup got it up and running,I will give that a try,makes me wish I could read the manual in the language it was written in,wonder what else we are missing.

Adrenalynn
04-14-2008, 06:50 PM
Is the manual available for download?

If it's not terribly huge, I'd be willing to have a look at it. Linguistics is my main hobby/passion - there's a good chance that if it's far eastern or pacific rim that I'm fluent enough to translate.

trey3670
04-14-2008, 09:55 PM
http://www.robotis.com/html/main.php
I wouldnt want to put you out but if your bored.......and thanks tom! works!

Adrenalynn
04-14-2008, 10:51 PM
I see the manual for the CM-2+ in English, honestly the translation is probably near as good as anything I'd do, and my Pyojunmal/Hangungmal (South Korean) is pretty good.

Is there a model you're looking for that isn't in English?

[edit: actually, it's really darned good - I'm impressed...]

trey3670
04-14-2008, 11:28 PM
nope,thanks! appreciate you taking time to look through it!

Adrenalynn
04-14-2008, 11:50 PM
I'll read through the original version and make sure it doesn't have anything additional to it.