PDA

View Full Version : Sensor bot


4mem8
04-24-2008, 05:21 AM
This is a sensor robot and as the name implies it has a number of sensors.
[1] IRPD sensor
[2] GD2P12 IR sensors
[3] bump micro switches
[4] PIR
[5] Ping Ultra sonic
[6] CDS for LED headlights

None sensor
[7] Emic text to speech
[8] Pan/tilt
[9] Co-Processor [Bluebell design]

This project took about 6 months to complete and is not yet finished programing wise.

Check out the CO-Processor specs here:
http://www.bluebelldesign.com/CoProcessorFeatures.htm

http://img246.imageshack.us/img246/6777/43gf0.jpg


Below is a tutorial on how it was built

Pics to come

4mem8
04-24-2008, 06:04 AM
http://img153.imageshack.us/img153/5385/holesdrilledur1.jpg


Holes drilled for the servos,casters and main cpu boards.


http://img261.imageshack.us/img261/6721/paperremovedfromacrylicqo3.jpg


Paper removed from acrylic sheet.


http://img141.imageshack.us/img141/365/50863070do2.jpg




Placement of main CPU board


http://img141.imageshack.us/img141/6186/34902780hq6.jpg
Bluebell design co-processor board, The start of inserting components, Ic sockets and header pins.


http://img143.imageshack.us/img143/5273/21193818og6.jpg

Bluebells co-processor board, Electrolytic caps installed.


http://img530.imageshack.us/img530/9659/79855517mr3.jpg

Bluebells co_processor board, Resistors installed.

http://img177.imageshack.us/img177/9117/66473382mk6.jpg

Bluebells co_processor board, Underside.

http://img176.imageshack.us/img176/4853/10wu7.jpg

Parallax BS2P40 Demo board underside and alloy stand off brackets.

http://img176.imageshack.us/img176/8023/11uf2.jpg

Parallax BS2P40 Demo board with stand off alloy brackets.

http://img74.imageshack.us/img74/1580/12zf7.jpg

Parallax BS2P40 main board and BS2 syntax manual

http://img520.imageshack.us/img520/8931/13jg0.jpg

Two alloy brackets for holding the servos, Servos are continuous rotation type.

http://img132.imageshack.us/img132/4316/14md7.jpg

Servos and casters mounted.

http://img149.imageshack.us/img149/9893/17rm2.jpg

Wheels mounted to servos.

http://img512.imageshack.us/img512/7409/16xc7.jpg

Next a set of casters that match the height of the bottom of the servo wheel so that when the base sits flat on a table there is NO rocking of the base.

http://img132.imageshack.us/img132/2434/15fa7.jpg

Right side up and all mounted.

http://img520.imageshack.us/img520/8261/19yn6.jpg

4mem8
04-24-2008, 06:26 AM
http://img410.imageshack.us/img410/8605/41qm2.jpg


Soldering LED wires to co-processor board.

http://img84.imageshack.us/img84/4122/18zs8.jpg

Next we have fabricated an alloy bracket for the battery box which is fixed between the servos. The batteries are 2,500mah Enegizer recharghables.

http://img524.imageshack.us/img524/2118/26tx5.jpg

Next we have to make a bumper, this is fabricated from 1mm alloy with a SQ LEGO 4x4 block glued to the back of bracket and it uses the hole through the center for the rod support.

http://img442.imageshack.us/img442/9150/27ni0.jpg

These are our IRPD infra red distance sensors { Phillips ] Center one is the receiver and two outer ones are transmitters.

http://img442.imageshack.us/img442/275/28uy5.jpg


LEGO Technics parts used for the housing of the IRPD transmitters.

http://img185.imageshack.us/img185/3899/29wp4.jpg

The sensors are a perfect fit into the Technic parts.

http://img185.imageshack.us/img185/8519/emailirpdsensorfittedxv0.jpg

Receiver IRPD fitted center top, the four LEDS below are the headlights 8,000 MCD. [ Brightness]

http://img104.imageshack.us/img104/1001/24op1.jpg


This is my ping ultra sonic system with pan/tilt servos and Lynxmotion pan/tilt brackets, Ping from Parallax. 5mm acrylic base to mount pan/tilt on.

http://img104.imageshack.us/img104/8200/23op0.jpg

Side view of pan/tilt sensor.

http://img181.imageshack.us/img181/8657/37jn7.jpg

Top view showing pan/tilt fitted to the front and co-processor board.

http://img398.imageshack.us/img398/3857/25ro6.jpg

Front view of pan/tilt.

http://img524.imageshack.us/img524/4774/31cr6.jpg

GD2P12 IR distance sensors and alloy brackets.

http://img72.imageshack.us/img72/3030/32fl7.jpg

PIR [ passive infra red ] from Parallax and mounting bracket.

http://img104.imageshack.us/img104/2599/36dw1.jpg

Bumpers and sensors in place.

http://img236.imageshack.us/img236/7215/20xw7.jpg


Main BS2P40 Demo board and sensors in place.

http://img410.imageshack.us/img410/1350/39xo2.jpg


Rear view of GD2P12 sensor.

http://img245.imageshack.us/img245/195/34pj0.jpg

Another rear view.

4mem8
04-24-2008, 06:31 AM
http://img76.imageshack.us/img76/4818/53rm8.jpg

Scm [ servo control module ] top left and Emic speech processor mid left, most wiring now complete.

http://img153.imageshack.us/img153/925/50po4.jpg

Battery pack for LED headlights [ blue ] Top right is a future add on, Line following circuit board.

http://img294.imageshack.us/img294/443/55ij6.jpg

Left view

http://img169.imageshack.us/img169/2425/44lb3.jpg

Work completed to date

More to come

2007 © 4mem8

archcvd
04-24-2008, 12:23 PM
Fantastic! I really like the step-by-step you provided too.

4mem8
04-24-2008, 03:21 PM
Archcvd: your welcome, Hope everyone enjoys it.

Tyberius
04-24-2008, 03:57 PM
Very nice write up, I like that you did a step by step, I should really do something similar on my next bot.

4mem8
04-24-2008, 04:03 PM
Tyberius: Many thanks for your comment, It is time consuming doing a detailed write up but I think well worth it for the viewers. As they can see what is involved in building a robot, whether simple or complex. I would love to see a detailed tutorial of your bots. Although your J5 is pretty good.