View Full Version : Galvanometer instead of Servo?
B.Glen
04-27-2008, 09:05 AM
Has anyone ever used a moving coil galvanometer (volt meter) instead of a servo? Would it work as a silent alternative? Any ideas about control issues?
lasernerd
05-10-2008, 12:35 PM
For what purpose?
each have there high points
Adrenalynn
05-10-2008, 12:43 PM
>> each have there high points
That's the point where you elaborate on your opinion, Laser'
lasernerd
05-10-2008, 01:16 PM
>> each have there high points
That's the point where you elaborate on your opinion, Laser'
in which application??
A galvo is a more precise movement
Where a servo has more power less precision
based on many factors
"just my opinion"
galvo's depend on optical sensors "closed loop"
for position detection
servo's use a mechanical means for postion detection
or optical counting
for meter movement obviously you dont need optical detection for scale,,
Adrenalynn
05-10-2008, 01:32 PM
So they could very well work as a "silent alternative" for lighter torque applications. I'm sure there are other options for detecting position outside of optical. A potentiometer comes to mind.
What control issues might the OP face?
lasernerd
05-10-2008, 01:41 PM
So they could very well work as a "silent alternative" for lighter torque applications. I'm sure there are other options for detecting position outside of optical. A potentiometer comes to mind.
What control issues might the OP face?
A pot is mechanical
Optical position can be impaired by dust, ext. light illumination
yes,for sure a galvo can be very quit at lower speeds
but at 40K points per second they can become squealer!
Adrenalynn
05-10-2008, 01:55 PM
Sealed optical positioning is immune to both forms of impairment you note, and would probably be worth exploring in that application.
Sure, pots are mechanical. They're also a "good ol' standby", and with the "right" D/A can be quite worthwhile in some applications.
I've heard meters squeal, but they're still not as loud as an HS-805.. ;)
lasernerd
05-10-2008, 02:19 PM
yep,
thats why they have there own dutys
vBulletin® v3.8.1, Copyright ©2000-2010, Jelsoft Enterprises Ltd.