PDA

View Full Version : My Fire-Fighting Robot



lnxfergy
05-14-2008, 12:01 PM
I posted some details of my latest robot a few days ago, and some people wanted to see my other bots, so here goes:

This is Little Green Machine III, my entry to the 2008 Trinity Fire Fighting Contest. He placed 16th out of 42 in the senior division (I had some problems with sensors getting screwed up by really shiny walls... wasn't doing enough front end processing on the data).

http://home.nycap.rr.com/ferginfo/Robots/pictures/xrb4.jpg

LGM3 uses an ATMEGA16 as it's processor. 4 IR sensors plus a sonar give me 180 degrees of coverage in the front. A uvtron and pyroelectric are used for rough and fine finding of the flame.

http://home.nycap.rr.com/ferginfo/Robots/pictures/xrb4elec.jpg

While LGM3 isn't that spectacular of a mechanical innovation, his software is quite interesting. Most contestants use a hard coded set of instructions on where to go to get through the known maze, some even use simple wall following techniques. LGM3 uses a topological map, and a hybrid architecture where a central planner oversees and suppresses lower level reactive behaviors. The software is written in C and uses the AVR-GCC compiler.

I've been working on methods to improve the sensor data, and plan to probably re-enter him next year with the newer software.

-Fergs

Dave
05-16-2008, 03:39 PM
Neato. What pyroelectric sensor did you use?

lnxfergy
05-20-2008, 01:29 PM
Neato. What pyroelectric sensor did you use?

Thanks. I'm using the Eltec sensor from Acroname. I bought it about 5 years ago, when they were only reasonbly expensive at $50, last check they were pushing $80. It's a really nice sensor because, unlike most, the signal is already amplified to be 2.5V center, and 0-5V, rather than being in the millivolt range and requiring external amplifiers.

That said, I'm now playing with some IR photodiodes for my next robot, because $3-4 is a lot nicer than $80.

-Fergs