PDA

View Full Version : Daventech Sonar Mount


Sienna
06-05-2008, 06:38 PM
Does anyone know of a Daventech (SRF-04/08) sonar mount, that allows me to mount the sonar pointed "toward" the servo horn?

For instance, these mounts (http://www.trossenrobotics.com/store/p/3263-Servo-IR-Sensor-Bracket.aspx)mount the sensor pointed 'away' from the servo horn, I want to mount the sonar on the opposite face as they are shown.

Thanks!

LinuxGuy
06-05-2008, 09:14 PM
Does anyone know of a Daventech (SRF-04/08) sonar mount, that allows me to mount the sonar pointed "toward" the servo horn?
This would take a "U" shaped bracket, which would not be difficult to design with the proper mounting hole dimensions.

8-Dale

jes1510
08-08-2008, 02:27 PM
Can you not just mount them on the opposite side? The bracket looks like it has symmetric holes and should allow you to mount the sensor on the other face.

A-Bot
08-08-2008, 04:33 PM
It can be mounted facing the opposite way. You just have to drill holes on the opposite corners. For some reason they only drill two holes.