PDA

View Full Version : [Question(s)] Gp2y0d340k


lnxfergy
06-19-2008, 03:22 PM
Ok, so I just started looking at this sensor (I've used GP2D12s, 120s and 15s for years).

I've got the data sheet, but I'm a little confused. Digikey specs this as consuming 31mA, but the datasheet says to use a resistor of 1Ohm for the LED drive circuit and has note about the LED consuming 300mA on average. Now, I know the LED isn't on all the time (it likely has two carrier frequencies like other modules), but wow, 300mA?

Has anyone used this sensor before? I just want to know that 1Ohm is correct and that I won't blow up the LED inside.

http://document.sharpsma.com/files/gp2y0d340k_e.pdf

-Fergs