jarkman
02-18-2018, 09:36 AM
Hi - just put my Pincher together, went smoothly, I'm very pleased with it.
I had a bit of kit-feedback, just in case it is useful:
1 - The unplated 2mm nuts in the Pincher kit sometimes took a lot (really quite a lot) of force to fit into the AX-12s. I only worked out halfway through that the plated nuts supplied with the AX12s were a much better fit and went in with sensible force. Might be good to mention that in the otherwise-excellent instructions.
2 - The tube of Turbo Fuse in the kit had turned to jelly. I used a tiny amount of generic cyano as a substitute. We'll see if that was a good idea when I first have to take it apart... :-)
3 - One of the instructions referred to bolts that were not in the kit or the little parts list at the start of the section:
"Mount the Upper Deck to the Lower Deck using the standoff assemblies using 8 x M3*10 bolts."
I used M3*8, works fine.
4 - The gripper linkage arms needed a bit of flash cleanup from the holes before the bushes would fit, again might be worth mentioning in the instructions.
Hope that helps, thanks again for an awesome arm!
Richard
I had a bit of kit-feedback, just in case it is useful:
1 - The unplated 2mm nuts in the Pincher kit sometimes took a lot (really quite a lot) of force to fit into the AX-12s. I only worked out halfway through that the plated nuts supplied with the AX12s were a much better fit and went in with sensible force. Might be good to mention that in the otherwise-excellent instructions.
2 - The tube of Turbo Fuse in the kit had turned to jelly. I used a tiny amount of generic cyano as a substitute. We'll see if that was a good idea when I first have to take it apart... :-)
3 - One of the instructions referred to bolts that were not in the kit or the little parts list at the start of the section:
"Mount the Upper Deck to the Lower Deck using the standoff assemblies using 8 x M3*10 bolts."
I used M3*8, works fine.
4 - The gripper linkage arms needed a bit of flash cleanup from the holes before the bushes would fit, again might be worth mentioning in the instructions.
Hope that helps, thanks again for an awesome arm!
Richard