PDA

View Full Version : Sharp IR Sensor GPD120



BrandonG32
07-08-2008, 03:04 PM
Good evening guys,
Another question about a different sensor. For the Sharp IR sensor, what is the minimum and maximum analog value received by the Sensor to the board. I'm getting 0-616. My configuration is also that I made the wires longer by 10ft. Also is the values suppose to change when something stationary is in front of the sensor? For example, when an stationary object is in front of the IR, I read in 612,607,608,610,607,611,609. Also the equation to use to convert the 10 bit A2D Sharp sensor only works for 0-1023. Is there an equation to use for one that goes to 0-616? Thanks again. Also in the C API , is there a function that can change the sensitivity or resolution of the sensor. I've looked but wasn't able to find it. Thank you God bless.