PDA

View Full Version : [Just For Fun] Favorite ROBOT movie???


rpedro
07-27-2008, 12:20 AM
ok, which is it??? best of all time... so far mine has to be i-robot...:) I just love that movie...

Adrenalynn
07-27-2008, 12:24 AM
Terminator.

crabfu
07-27-2008, 01:58 AM
Lauta: the castle in the sky & Wall-E.... hard to choose between 2 of my favorite animation studios :)

-Crabfu

4mem8
07-27-2008, 02:57 AM
Terminator, J5, I-robot and I also like the Matrix robots in the last episode re-loaded.

sthmck
07-27-2008, 08:02 AM
In order from most fav. I Robot, Wall-e, Transformer, Terminator, and then Iron Man. Ok so Iron Man isnt about robots but it has them in it so it counts.

BADfish10
07-27-2008, 08:35 AM
Probably
I Robot (looks the most likely humanoid getup)
Terminator 1 (was just nails)
J5 (Got to love Tracks lazers, Dirty danceing)
Last not strictly a robot but Alian 2 the heavy lifter in the cargo bay

J

ScuD
07-27-2008, 04:20 PM
I kinda liked Virus... but I'd say it rates lower than I robot and Terminator though.

Droid Works
07-27-2008, 07:24 PM
I would have to say runaway was my fav.

MYKL
07-28-2008, 09:21 AM
Runaway was an awesome movie. The combination of the robots, and trick bullets and Gene Simmons almost makes up for the crappy soundtrack.

I'm big into the Anime stuff also.

Black Magic M-66
GUNM
Patlabor
Appleseed

Star Wars, Teminator(s), RoboCOP and J5 were what hooked my interest in robotics the first place though.

metaform3d
07-28-2008, 01:17 PM
The Questor Tapes is a largely overlooked gem. I'd also given an honorable mention to 2001 and The Forbin Project which -- although they don't specifically contain robots -- do feature computers that extend themselves into remote devices to go all Frankenstein on their creators.

There is a special place in robot hell for Tweaky and that kid from A.I.

Matt
07-28-2008, 01:25 PM
Matrix 4 me.

rpedro
07-28-2008, 11:15 PM
The first Matrix is such a great movie...

Alex
07-29-2008, 08:50 AM
All right, I'll bite;)



Star Wars (? hey, there were a TON of robots in it)
The Matrix
I-Robot
Terminator
WALL-E
Transformers
Short Circuit
Runaway

Tyberius
07-29-2008, 09:37 AM
Am I the only one who HATED I-Robot? :p

Adrenalynn
07-29-2008, 09:40 AM
There were robots in that movie? The only time I noticed them was when they got in the way of my viewing Will Smith.

rpedro
07-29-2008, 11:39 AM
There were robots in that movie? The only time I noticed them was when they got in the way of my viewing Will Smith.

now this is some funny stuff... hilarious...:D

LinuxGuy
07-29-2008, 10:09 PM
I would have to say runaway was my fav.
Runaway has always been one of my favorites and will remain on. Also Silent Running, Short Circuit (both), and I-Robot.

8-Dale