PDA

View Full Version : RoBard Test !!



uucww
09-03-2008, 08:30 PM
RoBard Test !!

DresnerRobotics
09-03-2008, 10:11 PM
Where did you purchase this from?

Can't wait to see more!

robot maker
09-03-2008, 11:35 PM
looks like a good board,but from the website its only 533 mhz 256 ram
what is the speed of the one you bought and memory


RoBard Test !!

4mem8
09-04-2008, 12:45 AM
1GHZ, and 1 gig ram, If you are refering to the Pico ITX, I have one also.

Adrenalynn
09-04-2008, 02:17 AM
That's not a PicoITX as you know 'em. It's an embedded board, running (if I'm not mistaken, it's covered by a lable) a Vortex86 processor, probably a Vortex86DX, which is basically a highly clocked 486DX processor. They can run up to (afaik) 800Mhz. I've seen them historically in the PC/104 form-factor.

Given the size, price, and performance of the C7 PicoITX, I have some trouble getting really excited about the embedded 486 boards these days, although I have a couple Geodes laying around.

4mem8
09-04-2008, 02:48 AM
I was refering to robot makers post Adrenalynn. [what is the speed of the one you bought and memory] Refering to Tyberious I think.

Adrenalynn
09-04-2008, 03:58 AM
I do believe he was talking to the OP (Original Poster), UUCWW, about the board that was posted in this thread, right? They're commonly 400-533mhz and limited to 256MB. You're the first to mention the PicoITX in this thread... ;)

4mem8
09-04-2008, 04:48 AM
Ah, just re-read it more carefully, sorry, you are right, I misinterpreted the post.

Adrenalynn
09-04-2008, 05:00 AM
No need to apologize! Some posts aren't all that clear to start with anyway... ;)

DresnerRobotics
09-04-2008, 08:16 AM
Given the size, price, and performance of the C7 PicoITX, I have some trouble getting really excited about the embedded 486 boards these days, although I have a couple Geodes laying around.

2w power consumption and some nifty built-in I/O ports. Would be fun to play with in the least, it's like a microcontroller on steroids.

uucww
09-04-2008, 05:05 PM
RoBoard & PICO-ITX

Adrenalynn
09-04-2008, 05:18 PM
How much of that Pico photo is port-adapters and power supply - neither of which are included in your "comparison" photo of the Vortex? :)

lucrecelu
09-04-2008, 08:56 PM
for more inforamation about RoBoard please visit www.roboard.com (http://www.roboard.com)
it is x86 PC based with 600MHz and 256MB on board, the CPU is Vortex86DX

uucww
09-05-2008, 06:52 PM
Regulators transformation !

uucww
09-06-2008, 10:59 PM
vga......................................

uucww
09-07-2008, 09:08 AM
cnc ......................

uucww
09-09-2008, 12:03 AM
cnc.......................................

uucww
09-11-2008, 02:14 AM
RoBoard‏ bios

uucww
09-14-2008, 12:11 PM
1.2V to 6.89V............

Adrenalynn
09-14-2008, 12:40 PM
This has got to be the most random thread I've seen here...

ooops
09-15-2008, 01:14 PM
This has got to be the most random thread I've seen here...

If a picture is worth 1,000 words, then this is a 19,000+ word thread.

Adrenalynn
09-15-2008, 01:18 PM
Unfortunately, they seem to be selected at random. ;)

uucww
09-17-2008, 09:42 AM
windows xp

uucww
09-22-2008, 12:24 AM
.................................................. .......:veryhappy:

uucww
09-22-2008, 03:30 PM
test............................

test---2....................................

dos test

uucww
09-22-2008, 11:31 PM
test-------------------