PDA

View Full Version : [Interesting] Robot junk yard



4mem8
09-07-2008, 07:08 AM
http://img291.imageshack.us/img291/4152/pict0050vk1.jpg



My robot junk yard, 4 robots out of 16 shown.

ooops
09-08-2008, 08:33 AM
4mem, I aspire to junk like yours!!!

BTW, is there a story behind the big guy toward the back corner of the bench?

Matt
09-08-2008, 10:51 AM
That is an ER1 from evolution. They don't make them anymore.

4mem8
09-09-2008, 04:21 AM
OOOPS/Matt:Yes the bot in the background is a modified ER1, I purchased this on Trademe.co.nz Similar to your E-Bay. It cost me $350 NZ basic kit, A real steal, I then ordered an arm, and two accessory kits, So have a large collection of ER1 bits. I talked to one of Evolutions engineers 6 months ago and he said that they were going to reintroduce a revamped ER1 kit around about now, so it will be interesting to see if this happends.

Nocturnal
09-09-2008, 11:11 AM
Ok, so you've got the ER1 at the back, the two halves off Wall-e on either side of ED-209, and I think that's J5's base, but whats that in front of the screen on the left hand side of the image?

4mem8
09-09-2008, 02:07 PM
He he, That's the upper torso of J5 lying face down., I am waiting for a heavy duty base bearing to replace the stock standard one which is not up to scratch with the modifications.Just above the Hitec servo programmer is J5's head camera's face down and left/right ,those white gears are the shoulders.