PDA

View Full Version : [Interesting] PIC GSM Cellular Development Board



Matt
09-11-2008, 11:53 AM
I saw this over in the Spark Fun blog and thought it was pretty cool.

http://www.sparkfun.com/commerce/product_info.php?products_id=8851


http://www.sparkfun.com/commerce/images/products/08851-03-L.jpg (http://www.sparkfun.com/commerce/product_info.php?products_id=8851)

Description: PIC-GSM is a great development board for cellular and remote monitoring applications. With it, you can easily monitor and control your home from anywhere there is cell phone coverage with your GSM cellular account. Insert any GSM SIM card and start accessing this board remotely over the cellular network.

Switch on and off relays remotely by SMS, monitor and toggle the status of any GPIO pin, speak or listen on the audio channel of the board, even monitor the built-in temperature sensor. The built-in GSM module has an on-board antenna allowing you to use this module as GPRS modem connected to your computer too. Panic button and alarm inputs can dial your phone and report for alarm or to send you SMS message.

Features:


ICSP/ICD connector for programming with PIC-MCP, PIC-MCP-USB, PIC-PG1,PIC-PG2, PIC-PG3 or PIC-PG4 and programming and debuggine with PIC-ICD2, PIC-ICD2-POCKET, PIC-ICD2-TINY
USB 2.0 type B connector allow board to be interfaced to PC host
GSM/GPRS Tri-Band module 900/1800/1900Mhz
Li-ion backup battery
PIC18F97J60-I/PT
GSM Audio In and Out
RS232 connector
Quartz crystal 20Mhz
Two relays 10A/250VAC
Two digital inputs
Analog input
Temperature sensor
5V voltage regulator
EXT connector for available GPIO
Four mounting holes 3,3 mm (0,13")
FR-4, 1.5 mm (0,062"), green soldermask, white silkscreen component print

Dimensions: 100x80 mm (3,9x3,15")

Adrenalynn
09-11-2008, 12:35 PM
I actually have one of those on my weather station at my house up in the mountains. Not the most sensitive receiver, but it does work pretty well. No good cell towers there, so I'm only getting about 2400bps with any repeatability - good enough for my application though!

RileyXave
10-31-2008, 02:24 AM
it is not the most sensitive receiver, but it does work pretty well...

MattPol
02-27-2009, 02:30 PM
Hi,
Our senior design recently purchased this development board. Does anyone have some sample code for some basic functions the board can do?