View Full Version : robosapien?
jes1510
10-01-2008, 03:35 PM
Has anyone considered modding a robosapien for Mech Wars? I don't have one and have never seen one first hand but it might be a relatively cheap way to get into the competition. This guy built something close:
http://www.engadget.com/2007/02/13/coilosapien-robosapien-mod-impresses-terrifies/
Tyberius
10-01-2008, 04:51 PM
Are they even a true biped? I always assumed they had rollers on their feet.
jes1510
10-01-2008, 05:41 PM
I don't think they have rollers. I believe they have a shuffling kind of gait.
Tyberius
10-01-2008, 05:44 PM
Go for it!
4mem8
10-01-2008, 06:06 PM
They do not have rollers Both V1 and V2 sway from side to side and shuffle forward, Would be hard to control the hand movement for weapons accurately enough to be of any use. I have both V1 and 2
elios
10-01-2008, 08:33 PM
that flame thrower looked pretty nice. i know how to make a better one..... honest!! but don't tell on me, please...
roschler
10-01-2008, 10:10 PM
A wrist mounted "squeeze your hand to trigger" weapon might work with the V2. The V2 is actually the unsung hero of the WowWee line. He his hands are very agile and combined with his ability to touch the ground, you can actually pick up fairly small items off the ground. I must admit though, I never got very good at using his hands until I remapped all the movements I needed to my Nintendo WiiMote. The factory remote control was just too complicated for me to use the V2's hand easily. Once I mapped all the relevant primary body movements to the WiiMote it became a lot easier to make good use of the V2's hands capability. I can't think of another robot, especially in the V2's price class, that even comes close in dexterity.
4mem8
10-01-2008, 11:09 PM
That's true roschler, your system with the Wiimote would be a lot better at controlling his arms and hands than the stock controller.
elios
10-01-2008, 11:54 PM
have you seen the u-tube videos with the guy using a wiimote interface with a PC? ill post some links shortly.
Adrenalynn
10-02-2008, 12:04 AM
I posted some videos here awhile back of using the Wiimote on the PC, but also using the Wiimote to drive a Traxster. Probably about 6-8mo ago.
elios
10-02-2008, 12:14 AM
okay. its a bit hard to get links from u-tube atm.... current matainence is going and the NZ site is all in Korean...
im not sure if it will work, didnt for me, not completely at least...;
YouTube - Low-Cost Multi-touch Whiteboard using the Wiimote (http://nz.youtube.com/watch?v=5s5EvhHy7eQ)
the software is open source for everyone
Adrenalynn
10-02-2008, 12:28 AM
That may be, but it won't drive a Traxster. :)
elios
10-02-2008, 12:39 AM
erm.. whats a traxter.... ?
Adrenalynn
10-02-2008, 05:04 AM
Google is your friend. :tongue:
http://www.roboticsconnection.com/p-15-traxster-robot-kit.aspx
jes1510
10-02-2008, 09:42 AM
I found this (http://www.robosapien1.com/resources/official-mod-guide/) page that talks about some mods being done to the Robosapien.
edit: This (http://home.planet.nl/~pruim006/index2.htm) page has a ton of info on how to mod or connect things to the robosapien.
vBulletin® v3.8.1, Copyright ©2000-2010, Jelsoft Enterprises Ltd.