PDA

View Full Version : [Project] BaR2D2 - Radio-controlled stocked BAR



jamiep
01-05-2009, 11:10 AM
This is my first post here and I thought I would show off my BaR2D2 project:

Goto:
http://www.instructables.com/id/Build_A_Mobile_Bar_BaR2D2/ (http://www.instructables.com/id/Build_A_Mobile_Bar_BaR2D2/)

That link takes you to the full build and video of it in action.

BaR2D2 is on the edge of greatness and I need YOUR help to win him some serious $$$! Bar2 is entered into The Craftsman Workshop of the Future Contest at Instructables. First prize is $20,000 in tools!!! As the contest entry closed last night, there are less than 200 entered! I like those odds!
25% of the score is based on public voting (i.e. YOU!)
PLEASE help a fellow botbuilder score BIG!
And vote for bar2 and rate BaR2's entry 5 stars. They may require that you enter an email address or something. Voting is only open this week.
PRETTY PLEASE? It will only take a minute!

Jamie Price

ooops
01-05-2009, 11:44 AM
Sorry Jamie, I voted for the duct tape organizer!
Just kidding ... no email address required. Now, if/when you win are you going to cut us in on the swag?
BTW welcome to the TRC, hopefully you will keep us up to date on the contest and the upgrades.

jes1510
01-05-2009, 12:10 PM
Voted. I'll take my payment in the form of a wrench set please. In all seriousness good luck. I have been following this robot for a while now and have been impressed with your workmanship.

Definitely stick around these forums. It's a pretty cool place.

No0bert
01-05-2009, 04:24 PM
Voted for you! The craftsmanship is astounding, good work!

But I keep going through it, you never mentioned where you got your base wheels, for the chassis?

revoltage
01-06-2009, 07:53 AM
I have an account there...I voted for you...hope you win :)

metaform3d
01-11-2009, 07:25 PM
BaR2D2 is a beautiful piece of robotic cabinetry. Good luck!

Rudolph
01-11-2009, 09:56 PM
Congrats on slashdot too ;)