PDA

View Full Version : MATILDA ROBOT for sale


MIR
02-13-2009, 04:16 PM
Hi! I have a fully functional MATILDA Robotic Platform for sale - it comes with a Briefcase Operator's Control Unit, Manipulator Arm with zoom camera, additional camera and light mount and 2 battery chargers. This unit was used by the National Guard of Louisiana, purchased in 2002 and sold as surplus. I have repaired the LCD screen on the control unit - I believe this is the only thing that was wrong with this unit. I am no expert, but have easily gotten all cameras to work and the little guy to do 360s. It has a total of 5 cameras included.

I have listed it on Ebay for a reasonable starting bid and wanted to inform the Trossen Robotics Community of its availability. The link to the auction is: http://cgi.ebay.com/ws/eBayISAPI.dll?ViewItem&ssPageName=STRK:MESELX:IT&item=350168841546

If you have any questions about it, just let me know.

Thanks!

Michelle

Adrenalynn
02-13-2009, 05:01 PM
[Moved to Garage Sale]

Quantum
02-13-2009, 09:58 PM
Thats cool