Connor
02-13-2009, 04:24 PM
I have a question with regard to these two servos..
According to the specs the 5990 can do 180 degrees by doing 600-2400us. Stock they're 120 degrees.
The 5995's do 180 degree on 1100-1900us. Can the 5995's be programmed to do 600-2400us for 180 degrees or 5990's be programmed to be the same as 5995's?
My problem is this.. I have a odd number of servos.. and I need to either get one more 5995 (which is disco'd), or trade that one in and get 2 5990's.. Cause, I really don't think mixing the two types in a biped will work very well unless it's matched on the other side.
Thanks, Connor
According to the specs the 5990 can do 180 degrees by doing 600-2400us. Stock they're 120 degrees.
The 5995's do 180 degree on 1100-1900us. Can the 5995's be programmed to do 600-2400us for 180 degrees or 5990's be programmed to be the same as 5995's?
My problem is this.. I have a odd number of servos.. and I need to either get one more 5995 (which is disco'd), or trade that one in and get 2 5990's.. Cause, I really don't think mixing the two types in a biped will work very well unless it's matched on the other side.
Thanks, Connor