Toymaker
03-09-2009, 03:35 PM
This is the first robot that I ever built, it must have been around the late seventies. Servo magazine, did a piece on this a few years back.
It was programmed using tones (decoded by PLL chips) playback by cassette player. Note the early ultrasonic ranger, the first I ever designed!
http://forums.trossenrobotics.com/picture.php?albumid=49&pictureid=193
This full sized robot was heavy and ran off a heavy duty car battery. It was before microcontrollers and I wanted to program it to do simple stuff, so I built a car stereo player into the front of the machine. I then built a 16 channel RC system based on sending audio tones that a bank of NE567 PLL chips decoded. The system was first started from a know point "Robot cubby hole" then sending the tone commands (via radio) over to the robot (tone1 = forward, tone5 = left arm up etc). At the same time, these tones (and the duration of the tone) was recorded on one channel of the stereo cassette, I used the other channel to record speech at certain parts of the playback. So when programming the robot, you first took it through the sequence that you wanted it to do later, then when finished, put the robot back at the start position, rewind the cassette and insert it into the robot who would now follow all the original tone commands.
Anyone else here build robots back then?
Tony
It was programmed using tones (decoded by PLL chips) playback by cassette player. Note the early ultrasonic ranger, the first I ever designed!
http://forums.trossenrobotics.com/picture.php?albumid=49&pictureid=193
This full sized robot was heavy and ran off a heavy duty car battery. It was before microcontrollers and I wanted to program it to do simple stuff, so I built a car stereo player into the front of the machine. I then built a 16 channel RC system based on sending audio tones that a bank of NE567 PLL chips decoded. The system was first started from a know point "Robot cubby hole" then sending the tone commands (via radio) over to the robot (tone1 = forward, tone5 = left arm up etc). At the same time, these tones (and the duration of the tone) was recorded on one channel of the stereo cassette, I used the other channel to record speech at certain parts of the playback. So when programming the robot, you first took it through the sequence that you wanted it to do later, then when finished, put the robot back at the start position, rewind the cassette and insert it into the robot who would now follow all the original tone commands.
Anyone else here build robots back then?
Tony