PDA

View Full Version : [Bioloid] I was having fun until.......



sniperscope
05-11-2009, 08:31 PM
Hello Everyone:
This evening I was having a blast learning Robot Terminal, issuing commands to my boy and having a great time......then it happened. I saved several poses to get ready and show off to my wife. When I used the Play command, my little guy went through his poses and then contorted as if suffering from a heart attach and blew a fuse. My first reaction was "what the frack is this?"

Why would cause my boy to blow a fuse? Can anyone point me in the right direction to find the cause?
Thanks.V

MikeG
05-11-2009, 10:12 PM
Too much current through the fuse.

jes1510
05-11-2009, 10:41 PM
If it contorted then it stalled a bunch of motors causing the current to skyrocket.

darkback2
05-11-2009, 11:22 PM
its called demo mode...everything works till you try to show it off. unfortunately the only cure is to only use your robot when noone is looking...also...hope your boy is ok.

Obscene
05-23-2009, 02:43 PM
Nah, what happened was, you attempted to use the Mirror Pose option. I've yet to find a suitable purpose for "Mirror Pose" because it doesn't quite work the way it says it should. Robotis hasn't given an explanation either.

I blew a fuse the same way.