PDA

View Full Version : Videos of Firgelli L12 Actuators needed



badboi
08-07-2009, 02:31 PM
Hi,

I am looking for videos of the Firgelli L12 actuators with 100mm using 12 Volts under zero load.

there are three gearing options
1) 1:50
2) 1:100
3) 1:210

Does anyone have a video showing the speed of these actuators?
it would be very helpful in choosing which to go with

thanks

robologist
08-08-2009, 04:13 PM
Don't know which ratio it is, but imagine Firgelli could tell you.

YouTube - L12 FIRGELLI TECHNOLOGIES MINI LINEAR ACTUATOR

Adrenalynn
08-08-2009, 04:20 PM
Remember that that's no-load speed too...

badboi
08-08-2009, 04:41 PM
Thanks!

I have seen those but like you said there were no specs on it..thats why i posted here

Firgelli is on vacation for 2 weeks so there is noone there....

could someone post on this forum those three actuators?

thanks

dave

lnxfergy
08-09-2009, 01:05 AM
Thanks!

I have seen those but like you said there were no specs on it..thats why i posted here

Firgelli is on vacation for 2 weeks so there is noone there....

could someone post on this forum those three actuators?

thanks

dave

I'm not sure I've actually seen any of our regular visitors actually using these in a project. Further, I doubt anyone out there has all 3, or even more than one style. Do they give the raw RPM of the motor under load? I'd think that a straight out calculation would be more useful than videos of unknown loads/inconsistent setups...

-Fergs

Adrenalynn
08-09-2009, 02:27 AM
Ooops has one, but I've no idea which. I agree, the no-load setup doesn't mean anything at all in the real world.