View Full Version : [Question(s)] Automatic Door Opener
lostout024
11-19-2009, 08:27 PM
Just recently I picked up on Craigslist a mini Monster Energy Drink fridge, and have decided to possibly focus my college senior project around it. Ultimately, I would like to create a robot to fetch my drinks and bring them back to the couch for me, but first, as my robotics experience is still minimal, I have decided to initially build a system that when activated, opens the door to the fridge for me. I feel like using an electric linear actuator for this would be my best bet, however I am unsure of the best way to set this up (such as how to connect the fridge and fridge door with the actuator). I would appreciate any ideas anyone has on this...or even if you think I'm somewhat on the right track...
Thank You,
Justin
Honestly, for a senior project, I would try to think of some other ideas before moving forward with this one. The whole "robot that gets me a drink" thing has become a cliche, I've never seen it done well, and I personally don't find it to be that interesting anyway.
There are so many interesting things that can be done with robotics technology.
Suicidal.Banana
11-25-2009, 07:47 AM
Make the fridge itself be the robot :P
xk5JNs7KO30
(if u dont understand the fun in the above video, its related to this (http://tinyurl.com/9lhxyg))
robologist
11-27-2009, 03:51 AM
I love this one :
YouTube- Beer Robot
Another favorite, machines made by Jamie Hyneman of Mythbusters
YouTube- 7up commercial - improved vending machines
JonHylands
11-27-2009, 09:33 AM
If you're looking for something interesting to do with your fridge, why don't you turn it into a robot?
Add some wheels or tracks to the bottom, put some sensors on it, and have it come to you. Like the 7up commercial, but on a more realistic scale...
- Jon
vBulletin® v3.8.1, Copyright ©2000-2010, Jelsoft Enterprises Ltd.