PDA

View Full Version : For Sale: Complete Phoenix Hexapod



DresnerRobotics
01-06-2010, 02:14 PM
Hey all!

I have far too many robots, and my poor beloved Phoenix hexapod has been sitting on my shelf gathering dust for a number of months. It is very lightly used, essentially I played with it for a couple of charges when I first built it, and since then it has only been brought out for Robogames 2009 and iHobby 2009.

It is a completely assembled and tested Phoenix Hexapod, which comes with all hardware, Bot Board II, Basic Atom Pro, SSC-32, a pair of 6v NiMH batteries (2300mAh and 900mAh, servos/logic power), 12 HS-645MG servos, 6x HS-422 servos, and a PS2 wireless remote setup. It is the exact robot you see in the last 4 videos on the product page here: http://www.trossenrobotics.com/lynxmotion-phoenix-hexapod.aspx

I'm willing to let this go for pretty cheap, as I have another project in mind. I'm also going to throw in a servo pan&tilt unit, a pair of airsoft tank guns, and a free Vanadium Labs Mini Robocontroller (this is the board used for the scoring unit in Mech Warfare). Essentially, you would have a very nice head start on building a Mech Warfare capable hexapod entry with this.

I'm asking for $500 shipped to you anywhere in the continental US. Open to offers as well.


http://www.youtube.com/watch?v=cuYx-NBW61s

Quantum
01-06-2010, 03:13 PM
PM Sent

DresnerRobotics
01-06-2010, 03:46 PM
Sold!

nagmier
01-06-2010, 09:46 PM
Wow that was SWIFT! Nice snag Quantum

Adam
01-06-2010, 10:28 PM
Nice deal! That's a lot of robot for the $.