PDA

View Full Version : Phoniex Hexapod Kit For Sale



Quantum
01-19-2010, 01:55 AM
I recently picked this up from Tyberius.
http://forums.trossenrobotics.com/showthread.php?t=3782

We tested it at the shop when he dropped it off worked great.

I dont need the kit and most of the parts as I was mostly interested in the servos.

So Here it goes back on the board as a partial kit which comes with all hardware, Bot Board II, Basic Atom Pro, SSC-32 V2, a pair of 6v NiMH batteries (2300mAh and 900mAh, servos/logic power), and a PS2 wireless remote setup, servo pan & tilt unit, one airsoft tank gun, and all of the aluminum servo horns.

I am adding a Lynxmotion Visual Sequencer SEG program on CD V1.15 which can be updated to V1.16 here http://www.lynxmotion.com/Product.aspx?productID=443&CategoryID=15.

Servos are just needed to make a complete kit.

I'm asking for $260 shipped to you anywhere in the continental US.

Paul

DresnerRobotics
01-19-2010, 12:12 PM
I can vouch that everything here is in great condition :)

FlowbotX
01-19-2010, 07:12 PM
Interested in a partial purchase. See PM. Thanks.

Quantum
01-20-2010, 04:54 PM
I broke the sale up.
Sold.