PDA

View Full Version : Basic Atom proM and Atom Pro



4mem8
02-11-2010, 10:34 PM
Ok question for the trained ppl here, I have two Atom Pro chips, but both are different to look at, One is a Pro M and the other is a pro the only difference i can see is the placement of components aft of the main chip. Do both chips preform the same, is there any phyisical difference in what they do?. your help would be appreciated.

Quantum
02-12-2010, 01:21 AM
Mike

They are the same only difference is the processor running the board. They switched it up but same features running on the boards.
Thats why they might look different.

Paul

4mem8
02-12-2010, 02:56 AM
Ok cool thanks Paul, just needed to know for my own info.

elios
02-12-2010, 03:06 AM
are you Finally getting into programming :P

the Basic language is quite easy... i teach the guys PICAXE basic at school, and with a few new PICAXE chips coming out this year the PICAXE Range is going to become a lot more versitile.

Perhaps I should teach you some time?:wink:

Quantum
02-12-2010, 03:10 AM
I am pretty sure on this but if I'm wrong Im sure someone will chime in.

4mem8
02-12-2010, 07:56 AM
Hey Liam yeah i need all the help i can get on programming lol . :wink:

elios
02-12-2010, 03:53 PM
Hey Liam yeah i need all the help i can get on programming lol . :wink:

Well see you some time round 1:30... time to get some progress done!

Has anybody seen GWjax around at all?