PDA

View Full Version : Fission



Quantum
02-14-2010, 06:32 PM
I'm planning on making the games. Here's Fission a quad based on the Prop with an IK engine. The gun I havnt completed yet as that is going to be self as well.

Servos:
HS-475HB
HS-645mg

Battery:
Lipo 1300 mah

Processor:
Single Prop Custom Board
Running IK Program

Control:
Xbee Or PS2 depending on program that is loaded.

Guns:
Custom 6mm airsoft gun.

Camera:
Undecided

Pictures below.
Movie in a couple days tweaking the gaits.

Paul

4mem8
02-14-2010, 07:51 PM
Cool project Paul, looking very neat indeed.love to see vid when u have it going. Nice work.

Adam
02-14-2010, 11:03 PM
Sweet quad!

Zenta
02-15-2010, 04:45 AM
Great work!
I love the leg design.

Good luck with this project.

-Zenta