PDA

View Full Version : Mini-Guns for my mech.



Connor
02-18-2010, 12:44 PM
Hey Guys.. I just wanted to show this off.. I didn't build these.. I asked gdubb2 to build them for me (I'm a bit sort on time these days).. I just want to say, he did a kick a$$ job on these and they're completely awesome.

http://forums.trossenrobotics.com/gallery/files/1/6/4/2/100_2392.jpg


http://forums.trossenrobotics.com/gallery/files/1/6/4/2/100_2393.jpg

http://forums.trossenrobotics.com/gallery/files/1/6/4/2/100_2395.jpg

I have two of them, and they're getting mounted to my bioloid humanoid for mech-warefare. They're just freaking awesome. BTW, my pictures don't do them justice either!

Thank you SO much gdubb!! Great work!

Thanks, Connor

webgeek
02-18-2010, 06:37 PM
Ha! Those look totally great!

jes1510
02-18-2010, 07:16 PM
Man, those are gorgeous! Awesome work GDubb!

4mem8
02-18-2010, 08:07 PM
Awsome work GDubb, Have a friend making me some working ones different to above for my T! Rotating barrels and firing. but those look real cool GDubb.

gdubb2
02-18-2010, 08:42 PM
Hey all,
Thanks for the comments. Now guns with rotating and firing barrels would be something. I've seen vids of them, but to make one would be fun. Especially light enough for a Mech..(In my dreams)

Gary

4mem8
02-18-2010, 11:43 PM
Hey all,
Thanks for the comments. Now guns with rotating and firing barrels would be something. I've seen vids of them, but to make one would be fun. Especially light enough for a Mech..(In my dreams)

Gary

Yeah they are awesome to see, but one for a mech and light enough could be a problem.

zoomkat
02-19-2010, 12:22 AM
One might could make the barrels so that the real barrel is in the center of the fake barrels, then have the fake barrels spin around on the real barrel using one of those small thin vibrator type motors.

sthmck
02-19-2010, 12:47 AM
One might could make the barrels so that the real barrel is in the center of the fake barrels, then have the fake barrels spin around on the real barrel using one of those small thin vibrator type motors.

Good call, I was thinking the exact same thing.

DresnerRobotics
02-19-2010, 02:05 AM
So when does Gdubb's shop open? lol

rebel
02-24-2010, 10:11 AM
That is an awsome looking weapon

bonmot
03-08-2010, 10:50 AM
Wow, what an art work!
It is spring loaded, or powered by mini CO2 tank?
I am asking because I play paintball!

SN96
03-10-2010, 06:11 PM
Those look awesome. I wanted to make something like this but have it where it rotates and fires. I have a few ideas on how to possibly make one but it wouldn't be very strong or shoot very far. It would be more for effect than preformance. Size and weight make it hard to come up with a design that shoots with power and speed.

What you have is still a great design and practical.
________
XT600 (http://www.cyclechaos.com/wiki/Yamaha_XT600)