PDA

View Full Version : Dynamixel AX12 with phidgets



danhoskin
03-05-2010, 05:25 AM
Is the AX12 servo compatible with phidgets servo controllers?

DresnerRobotics
03-05-2010, 10:01 AM
Nope, those can only control standard hobby servos. The ax-12s call for a half duplex UART, which isn't provided on any phidgets device.

Tekkadon
05-14-2013, 06:01 AM
If you are using phidgets, you might have USB ports anyway and use the Dynamixel to USB converter in addition to your phidgets.

KevinO
05-14-2013, 04:35 PM
Xevel's USB2AX is also an option. If you are only using AX or MX servos it is in my opinion a better choice than the USB2Dynamixel.

jwatte
05-14-2013, 05:15 PM
Yeah, the USB2Ax is not only slightly cheaper, but it also has proper protection of the input/output serial bus; overvolting and spikes won't render it permanently useless like the USB2Dynamixel.