PDA

View Full Version : [Question(s)] Controlling SSC-32 with Atmega 168



sam
03-15-2010, 07:25 PM
Ok, So I have been tackling this issue for way too long so I decided to ask for help.

Info : I'm writting code in avr studio in GCC

I'm trying to comunicate with the Tx Rx lines (TTL I think it's called). The Tx line on my Atmega 168 is connected to Rx on the SSC-32. The baud rate on the SSC-32 is set to 9600 (I also tried 38.4k). The ground lines are connected to each other. I have very close to 5 volts on both the SSC-32 and the AVR.

In terms of program, I used basicly the program for the 50$ robot on Society of Robots. Here is what I have:


/************************************************** **************************
*
* Copyright (c) 2007 www.societyofrobots.com
* (please link back if you use this code!)
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*
* Alternatively, this software may be distributed under the terms of BSD
* license.
*
* Photovore v1, March 10th, 2007
* Simple case-based method for a robot that chases light.
*
*
************************************************** **************************/

//SoR Include
#include "SoR_Utils.h" //includes all the technical stuff


int main(void)
{
//declare variables here
//int i=250;//a 'whatever' variable
int sensor_left=0;//left photoresistor
int sensor_right=0;//right photoresistor
int threshold=8;//the larger this number, the more likely your robot will drive straight


/****************INITIALIZATIONS*******************/
//other stuff Im experimenting with for SoR
uartInit(); // initialize the UART (serial port)
uartSetBaudRate(9600);// set the baud rate of the UART for our debug/reporting output
rprintfInit(uartSendByte);// initialize rprintf system

//timerInit(); // initialize the timer system

configure_ports(); // configure which ports are analog, digital, etc.
a2dInit(); // initialize analog to digital converter (ADC)
a2dSetPrescaler(ADC_PRESCALE_DIV32); // configure ADC scaling
a2dSetReference(ADC_REFERENCE_AVCC); // configure ADC reference voltage

//rprintf("Initialization Complete\r\n");
/**************************************************/


/*********ADD YOUR CODE BELOW THIS LINE **********/
LED_off();//turn LED on




rprintf("#0P1500"); // I also tried sending each caracter seperatly...



while(1)
{



}
/*********ADD YOUR CODE ABOVE THIS LINE **********/

return 0;
}


/*********************COMMAND LIST*************************

delay_cycles(cycles);
Delays - you can make your robot wait for a certain amount of time with this function.
Put the number of computational cycles to delay in the ().
23 cycles is about .992 milliseconds
to calculate: 23/.992*(time in milliseconds to delay) = cycles
Check servo datasheet where it says: 'Direction: Clockwise/Pulse Traveling 1500 to 1900usec'


servo_left(speed); and servo_right(speed);
Commands your servos to rotate at a certain speed.
Vary speed (which represents a delay in cycles) from 20 to 50.
Left is for port D0 and right is for port D1.


LED_on(); and LED_off();
Turns on and off your LED. The LED is on port D4.
By bringing port D4 low, you are turning on the LED.


variable=a2dConvert8bit(pin);
Reads analog pin. For example, set 'pin' to 5 to read PC5.
'variable' will store the value.

************************************************** *********/


And there are two warnings when I build the code. They are in the uart.c file, so here it is :



/*! \file uart.c \brief UART driver with buffer support. */
// ************************************************** ***************************
//
// File Name : 'uart.c'
// Title : UART driver with buffer support
// Author : Pascal Stang - Copyright (C) 2000-2002
// Created : 11/22/2000
// Revised : 06/09/2003
// Version : 1.3
// Target MCU : ATMEL AVR Series
// Editor Tabs : 4
//
// This code is distributed under the GNU Public License
// which can be found at http://www.gnu.org/licenses/gpl.txt
//
// ************************************************** ***************************

#include <avr/io.h>
#include <avr/interrupt.h>

#include "buffer.h"
#include "uart.h"

// UART global variables
// flag variables
volatile u08 uartReadyTx; ///< uartReadyTx flag
volatile u08 uartBufferedTx; ///< uartBufferedTx flag
// receive and transmit buffers
cBuffer uartRxBuffer; ///< uart receive buffer
cBuffer uartTxBuffer; ///< uart transmit buffer
unsigned short uartRxOverflow; ///< receive overflow counter

#ifndef UART_BUFFERS_EXTERNAL_RAM
// using internal ram,
// automatically allocate space in ram for each buffer
static char uartRxData;
static char uartTxData[UART_TX_BUFFER_SIZE];
#endif

typedef void (*voidFuncPtru08)(unsigned char);
volatile static voidFuncPtru08 UartRxFunc;

// enable and initialize the uart
void uartInit(void)
{
// initialize the buffers
uartInitBuffers();
// initialize user receive handler
UartRxFunc = 0;

// enable RxD/TxD and interrupts
outb(UCR, BV(RXCIE)|BV(TXCIE)|BV(RXEN)|BV(TXEN));

// set default baud rate
uartSetBaudRate(UART_DEFAULT_BAUD_RATE);
// initialize states
uartReadyTx = TRUE;
uartBufferedTx = FALSE;
// clear overflow count
uartRxOverflow = 0;
// enable interrupts
sei();
}

// create and initialize the uart transmit and receive buffers
void uartInitBuffers(void)
{
#ifndef UART_BUFFERS_EXTERNAL_RAM
// initialize the UART receive buffer
[U]bufferInit(&uartRxBuffer, uartRxData, UART_RX_BUFFER_SIZE);
// initialize the UART transmit buffer
bufferInit(&uartTxBuffer, uartTxData, UART_TX_BUFFER_SIZE); // apparently he warning is here
#else
// initialize the UART receive buffer
bufferInit(&uartRxBuffer, (u08*) UART_RX_BUFFER_ADDR, UART_RX_BUFFER_SIZE);
// initialize the UART transmit buffer
bufferInit(&uartTxBuffer, (u08*) UART_TX_BUFFER_ADDR, UART_TX_BUFFER_SIZE);
#endif
}

// redirects received data to a user function
void uartSetRxHandler(void (*rx_func)(unsigned char c))
{
// set the receive interrupt to run the supplied user function
UartRxFunc = rx_func;
}

// set the uart baud rate
void uartSetBaudRate(u32 baudrate)
{
// calculate division factor for requested baud rate, and set it
u16 bauddiv = ((F_CPU+(baudrate*8L))/(baudrate*16L)-1);
outb(UBRRL, bauddiv);
#ifdef UBRRH
outb(UBRRH, bauddiv>>8);
#endif
}

// returns the receive buffer structure
cBuffer* uartGetRxBuffer(void)
{
// return rx buffer pointer
return &uartRxBuffer;
}

// returns the transmit buffer structure
cBuffer* uartGetTxBuffer(void)
{
// return tx buffer pointer
return &uartTxBuffer;
}

// transmits a byte over the uart
void uartSendByte(u08 txData)
{
// wait for the transmitter to be ready
while(!uartReadyTx);
// send byte
outb(UDR, txData);
// set ready state to FALSE
uartReadyTx = FALSE;
}

// gets a single byte from the uart receive buffer (getchar-style)
int uartGetByte(void)
{
u08 c;
if(uartReceiveByte(&c))
return c;
else
return -1;
}

// gets a byte (if available) from the uart receive buffer
u08 uartReceiveByte(u08* rxData)
{
// make sure we have a receive buffer
if(uartRxBuffer.size)
{
// make sure we have data
if(uartRxBuffer.datalength)
{
// get byte from beginning of buffer
*rxData = bufferGetFromFront(&uartRxBuffer);
return TRUE;
}
else
{
// no data
return FALSE;
}
}
else
{
// no buffer
return FALSE;
}
}

// flush all data out of the receive buffer
void uartFlushReceiveBuffer(void)
{
// flush all data from receive buffer
//bufferFlush(&uartRxBuffer);
// same effect as above
uartRxBuffer.datalength = 0;
}

// return true if uart receive buffer is empty
u08 uartReceiveBufferIsEmpty(void)
{
if(uartRxBuffer.datalength == 0)
{
return TRUE;
}
else
{
return FALSE;
}
}

// add byte to end of uart Tx buffer
u08 uartAddToTxBuffer(u08 data)
{
// add data byte to the end of the tx buffer
return bufferAddToEnd(&uartTxBuffer, data);
}

// start transmission of the current uart Tx buffer contents
void uartSendTxBuffer(void)
{
// turn on buffered transmit
uartBufferedTx = TRUE;
// send the first byte to get things going by interrupts
uartSendByte(bufferGetFromFront(&uartTxBuffer));
}
/*
// transmit nBytes from buffer out the uart
u08 uartSendBuffer(char *buffer, u16 nBytes)
{
register u08 first;
register u16 i;

// check if there's space (and that we have any bytes to send at all)
if((uartTxBuffer.datalength + nBytes < uartTxBuffer.size) && nBytes)
{
// grab first character
first = *buffer++;
// copy user buffer to uart transmit buffer
for(i = 0; i < nBytes-1; i++)
{
// put data bytes at end of buffer
bufferAddToEnd(&uartTxBuffer, *buffer++);
}

// send the first byte to get things going by interrupts
uartBufferedTx = TRUE;
uartSendByte(first);
// return success
return TRUE;
}
else
{
// return failure
return FALSE;
}
}
*/
// UART Transmit Complete Interrupt Handler
UART_INTERRUPT_HANDLER(SIG_UART_TRANS)
{
// check if buffered tx is enabled
if(uartBufferedTx)
{
// check if there's data left in the buffer
if(uartTxBuffer.datalength)
{
// send byte from top of buffer
outb(UDR, bufferGetFromFront(&uartTxBuffer));
}
else
{
// no data left
uartBufferedTx = FALSE;
// return to ready state
uartReadyTx = TRUE;
}
}
else
{
// we're using single-byte tx mode
// indicate transmit complete, back to ready
uartReadyTx = TRUE;
}
}

// UART Receive Complete Interrupt Handler
UART_INTERRUPT_HANDLER(SIG_UART_RECV)
{
u08 c;

// get received char
c = inb(UDR);

// if there's a user function to handle this receive event
if(UartRxFunc)
{
// call it and pass the received data
UartRxFunc(c);
}
else
{
// otherwise do default processing
// put received char in buffer
// check if there's space
if( !bufferAddToEnd(&uartRxBuffer, c) )
{
// no space in buffer
// count overflow
uartRxOverflow++;
}
}
}



The bold spot is the error...



The warning says : uart.c : 70 warning : pointer targets in passing argument 2 of "bufferInit" differ in signedness. soo... What does that mean exactly?

Thanks a lot for any infos you guys can give me, greatly appreciated. am I doing something wrong when sending stuff to the ssc-32?

Oh and BTW, I don't have a oscilloscope or actually anything to see if the AVR is sending data.

Sam