PDA

View Full Version : Remember that free Mechwarrior 4 announcement...



MSK Mech Commander
04-26-2010, 03:28 PM
At least they admitted that the announcement was premature by one year in the first sentence.:p
I can't wait for it to be released!

In the html it says it was posted on April 21st.

http://battletech.catalystgamelabs.com/2010/04/21/dare-we-say-it-free-release-of-mechwarrior-4-cleared-for-launch/

By the way, all of your mechs look awesome guys! Good luck at Robogames! I'll be devouring any videos that you post! :D

If you're wondering about my dormant status with my mech, that's about to end. Once I get free from some of my schoolwork and sports, I'll attack the situation violently.

I look forward to asking for help with my mech soon.

Stobs
04-26-2010, 04:25 PM
Is "MechWarrior 4" one and the same with the free "MechWarrior Living Legends"? Neither one mentions the other, but it doesn't make sense that there'd be two free products.
YouTube- MechWarrior: Living Legends - Beta Release Trailer

MSK Mech Commander
04-26-2010, 04:43 PM
I think that's the Mechwarrior that they are currently updating. They're redoing the whole Mechwarrior thing with improved everything, from what I've read.

They are only releasing Mechwarrior 4 for free.

DresnerRobotics
04-26-2010, 08:00 PM
Living Legends is a 3rd party effort Crysis mod, not an official title.

Stobs
04-26-2010, 08:26 PM
@Ty: /me nods yes, but it is sanctioned by MS [Edit], quoting the following from wikipedia: "Mechwarrior: Living Legends is a fan-created multiplayer mod (http://en.wikipedia.org/wiki/Mod_%28computer_gaming%29), based in the Battletech (http://en.wikipedia.org/wiki/Battletech) universe, and using CryEngine 2 (http://en.wikipedia.org/wiki/CryEngine_2) as its engine. It is one of the few mods to have been sanctioned by Microsoft (http://en.wikipedia.org/wiki/Microsoft)." Seeing how it's in a sense an open source project developed by fans-at-large then I'd have to conclude it actually is a separate product which, again, just seems strange to dilute the brand that way.