PDA

View Full Version : Spring Cleaning: Tri-Track, Arduino, Sensors



lnxfergy
05-17-2010, 03:12 PM
I've got a bunch of stuff that's just sitting around here doing me no good, priced to sell, hopefully others can put this stuff to use. I can only accept payment through paypal. All items will be shipped USPS (Continental US addresses only!). PM me if you are interested, first come, first served.

NOTE: ALL ITEMS IN GOOD WORKING CONDITION, HOWEVER DUE TO THE NATURE OF THE HOBBY, I CANNOT ACCEPT RETURNS, SINCE I CANNOT BE ASSURED YOU DIDN'T BLOW SOMETHING UP.

-Fergs

First up: I have 2 Pololu 3pi robots for sale, each comes with a black expansion deck (with LCD cutouts). These are nearly brand new, both in box, one still in wrapper inside the box, expansion decks are still in original plastic wrapping. Would be $110 new. Each is $70, shipped.

Next: A lynxmotion Tri-Track. Fully Assembled, never used (project it was intended for got canceled). $190 shipped. I will probably unbolt the center plates so that it fits easier into a box for shipment. Also includes small bag of hardware for attaching control boards.

http://forums.trossenrobotics.com/attachment.php?attachmentid=1924&stc=1&d=1274126499

Next Up: A solarbotics motors/tracks on Robotshop frame -- NO ELECTRONICS. Sells for $84 new, $60 shipped assembled and with motors already wired to go! The electronics shown are NOT INCLUDED. This little guy is in almost brand new condition.

http://forums.trossenrobotics.com/attachment.php?attachmentid=1928&stc=1&d=1274126499
http://forums.trossenrobotics.com/attachment.php?attachmentid=1929&stc=1&d=1274126499

Next: Set of 3 SRF-02 I2C sonar ranging sensors. Nearly new, with wires attached. $50 shipped.

http://forums.trossenrobotics.com/attachment.php?attachmentid=1931&stc=1&d=1274126499

Next up: Eltec Pyroelectric sensor (http://acroname.com/robotics/parts/R3-PYRO1.html), great for fire fighting robots or tracking people. This is not like your average Pyroelectric, it has a very high update rate. Brand new, sells for $95 from Acroname, $60 shipped.
http://forums.trossenrobotics.com/attachment.php?attachmentid=1484&stc=1&d=1252364334

Last, prototype frames from SMALdog. I've open sourced SMALdog's IK and motion engine (and NUKE will soon support custom 3DOF Mammal IK). I've got 4 extra frames, these are identical to SMALdog's. I don't particularly want to hang onto them, nor do I want to throw them out. May have extra holes in teh center of the platform, markings, etc. May show small stress cracks on bends, but are all plenty strong enough for building your own SMALdog. Probably also need to be cleaned up for sharp edges. $1 + $5 shipping = $6 shipped.

http://forums.trossenrobotics.com/attachment.php?attachmentid=1930&stc=1&d=1274126499

lnxfergy
07-02-2010, 09:40 PM
Prices reduced above. Also note, I can combine shipping on multiple items, so knock $5 off each subsequent item after the first.

-Fergs

lnxfergy
07-08-2010, 03:36 PM
SSC-32 and AVRISP2 are sold.

-Fergs

GWJax
07-09-2010, 11:16 AM
Thanks Fergs!! I can't wait to put them to good use.

Jax

lnxfergy
07-11-2010, 11:38 PM
Pololu Motors are gone.

-Fergs

Hellfire
07-20-2010, 12:01 PM
A lynxmotion Tri-Track. still available?

lnxfergy
07-20-2010, 12:41 PM
A lynxmotion Tri-Track. still available?

Yes it is.

-Fergs

lnxfergy
07-23-2010, 07:55 PM
Prices lowered on several of the remaining items above.

-Fergs