PDA

View Full Version : How many?



SteamAutomaton
06-03-2010, 01:25 PM
During a competition, how many batteries (and chargers) do people use?

SA:confused:

{Missing robot:confused}:p

Upgrayd
06-03-2010, 01:35 PM
I had four batteries and two chargers.

I could have gotten along with only two batteries and a single charger but it is much better to err on the side of caution.

If you are in some of the final rounds, or fighting your way back up through the losers bracket, you may end up having to run a few matches in quick succession.

sthmck
06-03-2010, 01:40 PM
I have three main batteries and three for my camera. By the end of Sunday I was using two chargers but I think that one should be fine.

gdubb2
06-03-2010, 01:45 PM
I have 3 complete sets of batteries, and 2 chargers. So far I really haven't needed to change much in between rounds, there seems to be enough time between matches to recharge. But as Upgrayed mentioned, it's better to err on the side of caution.

Gary

darkback2
06-03-2010, 01:48 PM
4 batteries...one charger, but I really didn't do that well...so I only had to swap batteries twice.